Search results for: 'ga-rew'
- GA-REW Air Blaster with Mini Blower GunStrong hitting force type of air shock gun. For spilling garlic seeds, removing thin skin of green onions, etc. Dust removal, draining, garlic seed spilling, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$269.90Min. 2 days
- GA-REW Line BlasterThis product has a smaller nozzle for a rotary type air shock gun, making it easier to install on a production line. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$169.90Min. 2 days
- GA-REW Air Mousse Gun Weakly Alkaline, Weakly Acidic Detergent CompatibleSpray the cleaning agent into foam on the mousse. The sprayed foam adheres to the vertical surface for a long time, floating dirt and cleaning. Car wash, food processing factory cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goods Suitable Fluid Weakly acidic to weakly alkalinefrom S$999.00Min. 8 days
- GA-REW Variable Shock Gun Rotating Type with GunEfficiently blows a wide area with the air injected from the rotating nozzle. The air injection diameter can be adjusted. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$389.90Min. 6 days
- GA-REW Precision Cleaning Brush Gun Nozzle UnitDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. Base cleaning, cleaning after various processing, cleaning of the inside of the car (panels, seats, mats, etc.), etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$389.90Min. 5 days
- GA-REW Air Blaster Nozzle UnitStrong hitting force type of air shock gun. Cleaning and dust removal after various processingRoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$289.90Min. 2 days
- GA-REW Variable Shock Gun Swing Type with GunEfficiently blows a wide range with the air injected from the swing nozzle. The air injection width can be adjusted. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$389.90Min. 6 days
- GA-REW General Cleaning Brush Gun Nozzle UnitDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. Cleaning of automobile / motorcycle parts, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$199.90Min. 5 days
- GA-REW Fine Deburring Brush Gun Alumina Nozzle OnlyThe synergistic effect of the air jetted from the rotating nozzle and the vibrating brush containing abrasive removes fine burrs such as dirt and resin. Precision parts molding, deburring of fine burrs after processing, etc. * The target burr is a micrometer-order beard burr. It cannot be expecte... Read MoreMaterial (Brush Part) Alumina (nylon base) RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$429.90Min. 8 days
- GA-REW Variable Shock Gun Swing Type Nozzle UnitEfficiently blows a wide range with the air injected from the swing nozzle. The air injection width can be adjusted. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$359.90Min. 6 days
- GA-REW Static Electricity Removal Brush Gun, Nozzle UnitDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. A conductive brush is used to suppress charging. Dust removal / cleaning during resin cutting, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$489.90Min. 8 days
- GA-REW Fine Deburring Brush Gun Silicon Carbide with GunThe synergistic effect of the air jetted from the rotating nozzle and the vibrating brush containing abrasive removes fine burrs such as dirt and resin. Precision parts molding, deburring of fine burrs after processing, etc. * The target burr is a micrometer-order beard burr. It cannot be expecte... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goods Material (Brush Part) Silicon carbide (nylon base)from S$479.90Min. 8 days
- GA-REW Air Blaster Mini Nozzle UnitStrong hitting force type of air shock gun. For spilling garlic seeds, removing thin skin of green onions, etc. Dust removal, draining, garlic seed spilling, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goods
- GA-REW Brushing CleanerIn addition to dry cleaning with air jetted from a rotating nozzle and a vibrating brush, water stains and semi-dry cleaning with mist spraying remove stains such as scale. Cleaning of automobiles / motorcycles, cleaning of returnable boxes, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$789.90Min. 6 days
- GA-REW Jet Streamer Hypochlorous Acid Water CompatibleSpecializes in spraying hypochlorite water. A blower using a 100V power supply spreads the chemical solution over a wide area. Sterilization / disinfection / antibacterial / deodorant spraying, pesticide spraying, etc.RoHS directive (corresponding to 10 substances) Correspondence Suitable Fluid Weakly acidic to weakly alkalinefrom S$1,299.00Min. 13 days
- GA-REW Static Electricity Removal Brush Gun, Gun TypeDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. A conductive brush is used to suppress charging. Dust removal / cleaning during resin cutting, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$559.90Min. 8 days
- GA-REW Air Mousse Gun Neutral Detergent TypeSpray the cleaning agent into foam on the mousse. The sprayed foam adheres to the vertical surface for a long time, floating dirt and cleaning. Car wash, food processing factory cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondence Suitable Fluid Neutral detergent Classification of the Hazardous Non-dangerous goodsfrom S$499.90Min. 6 days
- GA-REW Vortexer Weakly Acidic, Weak Alkaline Chemicals Drugs Compatible AgentProducts specializing in spraying photocatalysts, various coating agents, disinfectants and deodorants. Compatible with weakly acidic to weakly alkaline drugs Spraying photocatalysts, deodorants, etc., various cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$999.00Min. 2 days
- GA-REW Air Blow Blaster GunStrong hitting force type of air shock gun. Cleaning and dust removal after various processingRoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$349.90Min. 2 days
- GA-REW Variable Shock Gun Rotating Type Nozzle UnitEfficiently blows a wide area with the air injected from the rotating nozzle. The air injection diameter can be adjusted. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$359.90Min. 6 days
- GA-REW Mechanical Swing Nozzle UnitBy injecting air from a nozzle that swings its head from side to side, it has stronger striking power and saves energy compared to conventional flat nozzles. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$179.90Min. 2 days
- GA-REW Mr. Arashi Weakly acidic-weakly alkaline compatible typeUsing only the air from the air compressor, the liquid in the bottle is sucked up and sprayed into fine mist. Spraying sterilization, disinfection, antibacterial, deodorant, etc. (hypochlorite water, alkaline ionized water, etc.) * Cannot be used for spraying strong acids, strong alkalis, alcohol... Read MoreAir Pressure (MPa) 0.25~0.9 Connector Diameter Coupler plug 1/4from S$969.90Min. 8 days
- GA-REW Tornado 2Spray chemicals such as photocatalysts and deodorants into fine particles. It is also effective for cleaning the inside and outside of automobiles. Spraying photocatalysts, deodorants, etc., various cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goods Suitable Fluid neutralfrom S$579.90Min. 2 days
- GA-REW Fine Deburring Brush Gun Alumina with GunThe synergistic effect of the air jetted from the rotating nozzle and the vibrating brush containing abrasive removes fine burrs such as dirt and resin. Precision parts molding, deburring of fine burrs after processing, etc. * The target burr is a micrometer-order beard burr. It cannot be expecte... Read MoreMaterial (Brush Part) Alumina (nylon base) RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$479.90Min. 8 days
- GA-REW General Cleaning Brush Gun with GunDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. Cleaning of automobile / motorcycle parts, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$259.90Min. 5 days
- GA-REW Vortexer Waist Wearing Bottle TypeProducts specializing in spraying photocatalysts, various coating agents, disinfectants and deodorants. The spray gun and chemical bottle are separated to improve workability. Spraying photocatalysts, deodorants, etc., various cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$849.90Min. 8 days
- GA-REW Tornado Vacuum CleanerThe air ejected from the rotating nozzle knocks out dust and dirt such as mats, and sucks it with a vacuum cleaner. Cleaning car seats and mats, etc. * Vacuum cleaner is not included.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$639.90Min. 6 days
- GA-REW Precision Cleaning Brush Gun with GunDirt is removed by the synergistic effect of the air jetted from the rotating nozzle and the vibrating brush. Base cleaning, cleaning after various processing, cleaning of the inside of the car (panels, seats, mats, etc.), etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$429.90Min. 5 days
- GA-REW Vortexer Under Bottle TypeProducts specializing in spraying photocatalysts, various coating agents, disinfectants and deodorants. Spraying photocatalysts, deodorants, etc., various cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$679.90Min. 2 days
- GA-REW Fine Deburring Brush Gun Silicon Carbide Nozzle OnlyThe synergistic effect of the air jetted from the rotating nozzle and the vibrating brush containing abrasive removes fine burrs such as dirt and resin. Precision parts molding, deburring of fine burrs after processing, etc. * The target burr is a micrometer-order beard burr. It cannot be expecte... Read MoreRoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goods Material (Brush Part) Silicon carbide (nylon base)from S$429.90Min. 8 days
- GA-REW Mechanical Swing Nozzle with GunBy injecting air from a nozzle that swings its head from side to side, it has stronger striking power and saves energy compared to conventional flat nozzles. Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$229.90Min. 2 days
- GA-REW Air Shock Gun UnitEfficiently blows a wide range with the air injected from the swing nozzle. Specializing in installation on production lines Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondence Classification of the Hazardous Non-dangerous goodsfrom S$289.90Min. 5 days
- GA-REW Air Shock Gun with GunEfficiently blows a wide area with air injected from a rotating nozzle Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$199.90Min. 2 days
- GA-REW Vortexer Shoulder Bottle TypeProducts specializing in spraying photocatalysts, various coating agents, disinfectants and deodorants. The spray gun and chemical bottle are separated to improve workability. Spraying photocatalysts, deodorants, etc., various cleaning, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$849.90Min. 8 days
- GA-REW Air Shock Gun Nozzle UnitEfficiently blows a wide area with air injected from a rotating nozzle Dust removal, draining, etc.RoHS directive (corresponding to 10 substances) Correspondencefrom S$149.90Min. 2 days