100/90 tyre featured products
- DUNLOP TRAIL TYRES K950Lineup from hard road surface to soft road surface and all-round type. Can also be used off-road. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Display Pattern K950 Type WT
- DUNLOP SNOW TYRES (snow tire) D502A snow series that clears the theme of running through snowy roads at a high level. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Standard Rim Width (Inch) 1.60 Rim Diameter 17 Tire Size 2.50-17 4PR Display Pattern D502 Specification Front / Rear shared Type WT
- IRC IX series (IX-07S)Compatible with medium to soft road surfaces. [iX-05H] Higher block rigidity makes it easier to bite, and it is 100% effective even on sandy roads in fine weather. Due to the height of the block, it can easily handle the dry road surface expected in the latter half of the race. * We recommend tha... Read MoreDisplay Pattern IX07S Type WT
- TRUSCO Air Duster GunUses a large lever. The amount of blown air can be adjusted by operating the lever (0 to 100%). It has excellent oil resistance because it uses polyacetal resin for the main body. For drying, cooling, and dust work by air blow.Maximum Operating Pressure (MPa) 1 Connector Diameter 1/4 plug Nozzle Diameter (Φmm) 2
- IRC BR-99Enduro race tires that comply with FIM standards and can be driven on public roads. The high quality has been proven in numerous enduro races. It has both durability and grip, and demonstrates 100% of its performance from soft to hard road surfaces. * We recommend that you ask a maintenance compa... Read MoreDisplay Pattern BR99 Type WT
- Maruni Industry Air cylinderAir filling of tires for motorcycles and passenger cars * When using an air cylinder, the heat of vaporization may cause the temperature near the cylinder body and valve to drop sharply, resulting in frostbite. Be sure to wear gloves, etc., and do not touch the cylinder, valve area, etc. directly... Read Morefrom S$22.99Min. 2 days
- IRC MB520 URBAN MASTERAs the nickname of "Urban Master", it is perfect for running around the city with a sharp edge! It is ideal for middle scooters of 90-125cc class, and people who ride a scooter as a usual means of transportation such as "Running even in the rain, punk is troublesome" We will m... Read MoreSuitable for Front / Rear shared Display Pattern MB520 Type TL
- NGK Two-Wheeled Vehicle Racing Cable1. 1. High performance Made of silicon with outstanding durability, heat resistance, and withstand voltage. 2. High quality Ceramic resistors with extremely high noise suppression effect are used. 3. 3. A mold type cap that is highly reliable and 100% waterproof.Color Red Material Silicon
- KITACO Kevlar Drive BeltIn the crankcase, it is constantly adjusted by intense throttle work, and what is required for a drive belt that rotates at high speed while repeating pulling and bending is the strength above all. Next is the flexibility to follow acceleration and deceleration. Durability is also an important fa... Read More
- NASTA Push Open Register (with Pollen Removal Filter)It is a one-push method that can be opened and closed by simply pressing the push part lightly. With a pollen-compatible filter (20 μm pollen 90% removal), the intrusion of dust and dirt is greatly reduced. Since the front panel can be removed, it is easy to clean the inside such as the filter. *... Read MoreMaterial ABS Type Square register Color Silver gray Filter With filter for pollen removal
- DAYTONA Reinforced V-BeltA reinforced V-belt developed to support high power and high tune of sports scooters. The core wire uses * 100% aramid fiber. The belt length is set and quality controlled so that the reduction ratio is the same as the normal one when it is set on the pulley. * Some products use other core wire m... Read More
- NGK Ignition CoilWe provide ignition coils with excellent performance by using the advanced ignition system technology and strict quality standards cultivated over many years of NGK spark plugs. In an internal combustion engine that uses a spark plug, a high voltage of 20,000 to 35,000 V is required to discharge ... Read More
- BAL OHASHI Pantograph JackSG standard compliant productLowest Position (mm) 90from S$67.99Min. 2 days