18 rims featured products
- GLIDE Forged aluminum wheel [S18] R 450-17Glide is a Harley-Davidson wheel that has a simple and sporty design and generously introduced technology cultivated at Gail Speed, with the concept of "casual sports" that emphasizes price, quality and design. The S18 has 18 split spokes that balance rigidity and design, which is 5% li... Read Morefrom S$1,699.00Min. 2 days
- DUNLOP Vintage TireA traditional pattern that shines on a vintage-form machine with the elegance of a good era. We will convey the driving of the famous cars of the past with the feelings of the passionate men. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possib... Read MoreType WT
- TOYOTA MOTOR (73210) Front seat outer belt assembly right* After receiving your order, we may check the vehicle information. * Please note that we may cancel your order if it is difficult to obtain some registered products due to discontinuation or other circumstances after receiving your order due to the manufacturer's circumstances. * Depending o... Read Morefrom S$469.90Min. 2 days
- BRIDGESTONE HOOP B01 (Front / Rear shared)From customers who value economic efficiency to customers who are particular about driving and fashion. Scooter tire * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Display Pattern B01
- DUNLOP Buroro D605All-round trail tires that demonstrate stable driving performance from off-road to on-road. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Type WT
- IRC ON ROAD SPORTS DUROTOUR RS310 TyreA super long-selling model that has been loved by riders for about 20 years. Its popularity has not declined yet, not only in Japan but also overseas. With a wide variety of sizes, it can be installed on various bikes without any discomfort. As for the structure, by adopting a relatively tight R ... Read MoreDisplay Pattern RS310
- BRIDGESTONE BATTLAX SCBATTLAX SC pattern bias tire size lineup for scooters is newly expanded! * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- IRC MOBICITY SCT-001Next-generation model of scooter tires with excellent total balance. By adopting a high quality compound, the grip is improved on both dry and wet road surfaces while maintaining sufficient wear resistance. Compared to conventional products, the dry grip is 15% higher and the wet grip is 10% high... Read More
- MICHELIN SPORT TOU-RING PILOT ROAD3Pursuing further improvement of security under all weather conditions. "PILOT ROAD3" was developed with the goal of achieving both excellent grip performance and long-life performance under all weather conditions, which are required by users who mainly focus on sports touring. Tires in ... Read Morefrom S$289.90Min. 2 days
- Toyo-Sasaki Glass HS Stack Tumbler TumblerSpecification Oral physical enhancement Material Soda-lime glassfrom S$24.99Min. 2 days
- Toyo-Sasaki Glass Thin ice thin tumblerSpecification Full ion reinforcement Material Soda-lime glassfrom S$67.99Min. 2 days
- Toyo-Sasaki Glass USURAI On The Rock GlassCapacity (mL) 355 Top Diameter x Height H (mm) 80×80 Specification Full ion reinforcement product name/ type Shot glass Material Soda-lime glassfrom S$64.99Min. 2 days
- MICHELIN S1A large block shape is used for the pattern to ensure dry grip. The zigzag groove in the center part demonstrates high straight-line stability and excellent drainage performance. Uses a rubber compound to pursue excellent wear resistance. * We recommend that you ask a maintenance company to repla... Read Morefrom S$79.99Min. 2 days
- Toyo-Sasaki Glass Silkline on the rockCapacity (mL) 310 Top Diameter x Height H (mm) 74×85 Specification Full ion reinforcement product name/ type Shot glass Material Soda-lime glassfrom S$64.99Min. 2 days
- Toyo-Sasaki Glass HS Stack Tumbler Earthy SmokeCan be stacked.Capacity (mL) 250 TKG Part No. (2017) 6-2051-2101 Diameter (Φmm) 67 Top Diameter x Height H (mm) 67×95 TKG Part No. 8-2221-2101 Material Glass Types of tableware Western tablewarefrom S$22.99Min. 2 days