2010 honda odyssey parts featured products
- ENDY Antenna conversion cord HondaConverts Honda car antenna connector to standard (JASO standard) radio antenna plug. * When connecting the FM modulator, please use it together with EVC-4602 or EVC-4702.Cable coaxial cable Length (m) 0.2
- Aisin Seiki Water pump (Honda)* We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually. * Even if the model and engine model are the same, they may not fit depending on the model year. Be sure to check the genuine number.Manufacturer Honda
- GMB Water pump (for Honda)The water pump is an important part that circulates the coolant that cools the engine. The coolant, which has become hot due to the heat of the engine, is cooled by the radiator and returned to the engine. The water pump is located between the radiator and the engine, and is driven by a timing be... Read More
- Showa Auto Disc rotor (Honda)Rust-proof processing on the main body, rust-resistant disc rotor For passenger cars * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able t... Read More
- MK Kashiyama Disc PadA wide variety of raw materials are mixed in appropriate proportions using information accumulated over many years and quality engineering, and the effectiveness, life, squeal, vibration, and aggression of the mating material are met according to the requirements of the vehicle type, application,... Read More
- EXCEL Air Filter* Even if the model is the same, the type will differ depending on the model and year, so be sure to check the "genuine part number".
- MIYACO HYDRAULIC BRAKE MFG. Seal KitPiston seal for operating disc brake * Because it is made of rubber, it deteriorates due to the heat generated by the brake, which may cause the brake to malfunction or drag. * If you do not feel the brakes, we recommend that you check them once.
- BOSCH Air Filter Aeristo Premium (for Japanese Model)Anti-virus and allergen suppression functions have been added to the antibacterial type to further pursue comfort. It is effective in removing not only pollen and dust but also fine particles (PM2.5). * A separately sold tray is required for the first installation of vehicles without an air condi... Read MoreCross Reference Part No. (UNION) - Cross Reference Part No. (MICRO) -
- Union Sangyo (UNION) Cabin filterThe odor is caught by copper selgaia, which is made by crystallizing zeolite minerals that also exist in nature into cellulose fibers and has excellent gas adsorption properties. Adhere the dust collector and Sergeia with PE powder. Demonstrates dust collecting power without increasing wind resis... Read More
- Roadpartner Air filter* Please check the "genuine part number" as the type differs depending on the model and year even if the model is the same.
- ENDY Face panelThe clean and neat installation is proof of our commitment to sound. Compatible with each company's head unit, it completely hides the gap with the audio mounting port. * Please use in combination with the car component connector EJC-024N.
- MonotaRO Brake Pad NAO MaterialIt is a high-quality product manufactured by a domestic manufacturer that is used as a genuine product by a domestic car manufacturer. The material is non-asbestos and uses NAO material which is most suitable for domestic cars. * However, only the order code: 01080275 is made of low steel instead... Read More