B7hs-10 featured products
- NGK Spark Plug (B ~)Standard plug (plug for new car assembly) * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- NGK Iridium IX Plug for Two Wheeled VehicleIridium IX is an iridium plug that can be replaced with a standard heat value mounting (new car mounting) plug. Combustion spreads faster than general plugs, and a thermo-edge is provided at the tip of the insulator to improve plug fouling. A high-value-added plug that enables ignition, accelerat... Read More
- NGK Spark Plug for Two Wheeled VehicleThe center electrode has a "copper cored" structure in which copper is sealed close to the tip so that a large amount of heat can be released quickly. This provides an ultra-wide range plug that is resistant to burning and smoldering. Uses new ceramic insulator. The register plug has an... Read More
- DENSO Iridium Power Spark PlugWorld's smallest! Uses "0.4 mm" diameter iridium alloy center electrode. Reliable flight. Excellent ignitability. * The plug must be attached to the engine with the correct torque. * If the torque is too low, the engine and plug may be damaged due to leakage of combustion gas or loo... Read MoreResistor (kΩ) 5
- DAIHATSU (90919) Spark plug* After receiving your order, we may check the vehicle information. * Please note that we may cancel your order if it is difficult to obtain some registered products due to discontinuation or other circumstances after receiving your order due to the manufacturer's circumstances. * Depending o... Read Morefrom S$38.99Min. 2 days
- PROXXON Spark plug socket 1/2The driver system drive can be caught on the side instead of the corner, and stronger torque can be applied. The material is finished with chrome vanadium steel, and the hexagonal surface is guaranteed to be deep and uniform through forging. 2-year warranty for peace of mind! All items are marked... Read MoreSquare Drive (inch) 1/2 Square Drive (mm) 12.7 Specification Without magnet
- NGK Iridium Max PlugIt will be the iridium plug installed in the new car. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.
- KTC 9.5Sq Plug WrenchAdopted a new shape that is easy to distinguish from deep sockets. Comes with a magnet that prevents the spark plug from falling.Square Drive (mm) 9.5
- GMB Water Pump (For Daihatsu)The water pump is an important part that circulates the coolant that cools the engine. The coolant, which has become hot due to the heat of the engine, is cooled by the radiator and returned to the engine. The water pump is located between the radiator and the engine, and is driven by a timing be... Read More
- TOYOTA MOTOR (90919) Plug* After receiving your order, we may check the vehicle information. * Please note that we may cancel your order if it is difficult to obtain some registered products due to discontinuation or other circumstances after receiving your order due to the manufacturer's circumstances. * Depending o... Read More
- Honda Motor (50820) Rubber* After receiving your order, we may check the vehicle information. * Please note that we may cancel your order if it is difficult to obtain some registered products due to discontinuation or other circumstances after receiving your order due to the manufacturer's circumstances. * Depending o... Read More
- Union Sangyo (UNION) Cabin filterThe odor is caught by copper selgaia, which is made by crystallizing zeolite minerals that also exist in nature into cellulose fibers and has excellent gas adsorption properties. Adhere the dust collector and Sergeia with PE powder. Demonstrates dust collecting power without increasing wind resis... Read More
- Akebono Brake Industry Brake PadIt is a non-asbestos brake pad made by Akebono Brake. It is a pad that pursues quality, including OEM supply to automobile manufacturers. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you... Read More
- Amon Industry Plug WrenchGrip power is improved by adding appropriate unevenness to the surface. Even if your hands get oily, you can hold it firmly without slipping. For installing and removing spark plugs in automobiles Easy to turn with T-shaped grip. Check the plug size installed in the car. This product may not be u... Read MoreSize Overall length about 245mmfrom S$16.99Min. 2 days