Infrared heating element featured products
- YAC 3M insulation hard coatGreatly reduces the tingling sensation through the window. A transparent heat insulating film that you can feel the effect. 3M <Scotch Tint> auto film is used. (<3M> <Scotch Tint> is a registered trademark of 3M.) Achieves both high transparency and excellent heat insulation per... Read MoreWidth (mm) 500 × 1.5m roll Color Clear Reference Capacity For two light and compact carsfrom S$76.99Min. 2 days
- Canon Extender RF2XAn extender that is mounted between the "RF mount" camera body and the "RF lens" to extend the focal length of the lens. You can double the focal length of the attached lens. By adopting high refractive power and low dispersion glass material, various aberrations that cause de... Read MoreMass of Main Unit (g) 340 Overall Length (mm) 39.5 Maximum Diameter (Φmm) 71.2 Lens Configuration 9 elements in 5 groupsfrom S$1,399.00Min. 2 days
- Kaneka Kanelite Foam E1Excellent heat insulation performance. The gas was trapped in a small bubble of closed cells. As a result, the values of "convection, radiation, and conduction" of heat, which are known as the three elements of heat conduction, are fixed small. Closed cells block heat and suppress conde... Read MoreLiquid absorption 0.01g / 100cm 2 or less Thermal Conductivity (W/mk) 0.040 or less Moisture permeability coefficient (ng / m 2 sPa) 145 or less Linear expansion coefficient (cm / cm.℃) 6~8×10-5 Heat distortion temperature (℃) 80 (short term), 70 (long term) Dimensions, Width W x Length L (mm) 910×1820 Act on Promoting Green Procurement Conformity Formaldehyde grade F☆☆☆☆ Combustion Quality Pass Compressive strength (N / cm 2 ) over 20 Density (kg/m3) over 20 Bending strength (N / cm 2 ) over 20
- TERAOKA SEISAKUSHO Kapton Adhesive TapeA tape for electrical insulation and heat-resistant masking that is based on Kapton (polyimide film), which has excellent heat and cold resistance, mechanical properties, electrical properties, and chemical resistance, and is coated with a silicone-based adhesive. It can be used in various fields... Read MoreCore Diameter (mm) 75
- PEAK(Tokai Sangyo) Peak Loupe(No.1960) A modern loupe with a bright acrylic lens barrel. Practical equipment at home for general use. (No.1961) Consists of two Kellner. A versatile loupe that is bright, sharp and has ideal contrast. Ideal for inspecting negative film. (No.1962) Achromat with stable resolution, consisting of ... Read MoreMaterial (Lens) Glass Type Peak loupe
- HAKKO (Hakko Electric) Plug type heaterWith a protective tube for the sensor, equipment parts such as temperature controller overheating prevention can be easily attached. Since it is easy to install and handle and requires less installation space, the equipment cost is low and the structure is robust, so you can use it with confidenc... Read MoreDimension B (mm) 25 Material (Heater Sheath) C1220T (copper tube) nickel plating Protective Tube C1220T (copper tube) nickel plating Plug FC250 (iron casting) nickel plating Specification For water Material (Gasket) Non-asbestos (t1.5) Cap SPCC (paint)
- HAKKO (Hakko Electric) Ultra Five HL Type ( Heating Wire)High efficiency: A highly researched and highly accurate product that heats up without loss. Long life: High nickel alloy is used for the heating wire, and the original heat-resistant insulating magnesia is used, so the life can be significantly longer than that of conventional products. Robustne... Read More
- AS ONE Water HeaterIt is integrally molded with epoxy glass with excellent heat resistance and chemical resistance. Since heat is generated on the entire surface, the temperature rises quickly and the required liquid temperature can be obtained with less power. It can also be attached to plastic containers.from S$269.90Min. 2 days
- Mitutoyo Standard Cylinder GaugeUse by replacing with an appropriate anvil and washer according to the measurement dimensions. Cemented carbide is used at the tip of the stylus. Cemented carbide with excellent durability and wear resistance is used for the stylus and anvil. A foot rod (optional) can be used. * We do not deliver... Read MoreSeries 511
- AS ONE Immersion HeaterYou can easily heat the oil just by putting it in the oil and connecting the power supply. The stainless steel sheath has excellent corrosion resistance and can be used for alkaline solutions other than oil (liquids that do not corrode SUS316L).Power Cable (m) 2 (cabtyre cable with plug) Power Supply AC100V 50/60Hzfrom S$359.90Min. 2 days