Parts for toggle clamp.
* 1 set contains 2 sheets.
Trusco Part No. 765-2542 Outer Diameter (Φmm) 31 Suitable Screw Diameter (M) (mm) 12 Material Rolled steel for structural use Suitable Model TDJB2F Mass (g) 19
Side-push type toggle clamp. The push position can be adjusted with the bolt and nut at the tip.
For various fixing and temporary holding of metal and wood.
* Do not use for anything other than its intended purpose.
Clamping Pressure (kN [kgf]) 0.5[50] Base Flange Material (Handle) PVC Material (Main Unit) SS400 (Unichrome) Type Side push type
Downward pressure type toggle clamp. The push position can be adjusted with the bolt and nut at the tip.
For various fixing and temporary holding of metal and wood.
* Do not use for anything other than its intended purpose.
Type Downward pressure type Base Flange Material (Handle) PVC Material (Main Unit) SS400 (Unichrome)
Highly versatile downward presser type toggle clamp.
Ideal for inspection jigs, welding jigs, other assembly jigs, and processing jigs. Can also be used for woodworking and DIY.
The tightening pressure shown is a guide. The tightening pressure becomes weaker toward the tip of the clamp arm. Pleas... Read More
Small downward presser type toggle clamp.
Ideal for inspection jigs, welding jigs, other assembly jigs, and processing jigs. Can also be used for woodworking and DIY.
The tightening pressure shown is a guide. The tightening pressure becomes weaker toward the tip of the clamp arm. Please note that... Read More
Highly versatile downward presser type toggle clamp.
Ideal for inspection jigs, welding jigs, other assembly jigs, and processing jigs. Can also be used for woodworking and DIY.
The tightening pressure shown is a guide. The tightening pressure becomes weaker toward the tip of the clamp arm. Pleas... Read More
Vertical handle type downward pressure type toggle clamp. The push position can be adjusted with the bolt and nut at the tip.
For various fixing and temporary holding of metal and wood.
* Do not use for anything other than its intended purpose.
Type Downward pressure type Base Flange Material (Handle) PVC Material (Main Unit) SUS304
A lever with a grip that has excellent operability. The type with a safety lock has a specification that the lock functions at the clamp position. To release the lock, slide the grip cover and operate the lever, so there is no need to worry about releasing the clamp due to contact. The movable ra... Read More
Surface Treatment (Main Unit) - Material (Main Unit) SUS304 Material (Grip) polyamide Dimension P (mm) -
Downward presser type dual clamp. By adopting a cam mechanism in addition to the toggle mechanism and using an aluminum cutting body, durability, rigidity and performance have been dramatically improved. After the slide bar moves sideways from the main body, it moves downward and clamps.
Places w... Read More
RoHS directive (corresponding to 10 substances) Correspondence Mounting Flange Width (mm) Required for use: 30
Side-push type dual clamp. By adopting a cam mechanism in addition to the toggle mechanism and making the body stainless steel, durability, rigidity, and repeatability that are incomparable to toggle clamps have been dramatically improved. With self-lock.
Jig parts for machine tools such as machi... Read More
RoHS directive (corresponding to 10 substances) Correspondence Mounting Flange Width (mm) Required for use: 40
Hook type toggle clamp.
Clamp by hooking a fixed object with a U-shaped hook type bar. Machine parts Can be used as equipment parts.
The tightening pressure shown is a guide. Impact, vibration, and internal pressure may cause damage. Be careful not to get your hands caught.
Side-push type dual clamp. By adopting a cam mechanism in addition to the toggle mechanism and using an aluminum cutting body, durability, rigidity and performance have been dramatically improved.
Jig parts for machine tools such as machining.
* Cannot be used in hot places such as lathes and wel... Read More
RoHS directive (corresponding to 10 substances) Correspondence Mounting Flange Width (mm) Required for use: 30
A lever with a grip that has excellent operability. The type with a safety lock has a specification that the lock functions at the clamp position. To release the lock, slide the grip cover and operate the lever, so there is no need to worry about releasing the clamp due to contact. The movable ra... Read More
Dimension P4 (mm) - Dimension W4 (mm) - Dimension L4 (mm) - Dimension T (mm) 2.5 Dimension P2 (mm) 26 Material (Main Unit) SUS304 Material (grip cover) Thermoplastic elastomer (TPE) Movable range (°) [Arm] 86 / [Lever] 67 Material (Grip) polyamide
Since it is an assembly welding type, it can be set according to the site, and all are durable with a hardened bush. Downward presser type toggle clamp.
Ideal for applications that require durability. Ideal for welding jigs, other assembly jigs, and processing jigs.
The tightening pressure shown ... Read More
Side-push type toggle clamp.
Ideal for inspection jigs, welding jigs, other assembly jigs, and processing jigs. Can also be used for woodworking and DIY.
The tightening pressure shown is a guide. Impact, vibration, and internal pressure may cause damage. Be careful not to get your hands caught.