Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Eyebolt, W Screw

Eyebolt, W Screw
Sales Price: 2.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Hold the number line for stopping the piping
5
From Japan
On 2018-09-30 20:33:49
I think that the usability is good if the bolt part is longer by 10 mm more. It is full of nuts when attached to a 7 mm iron plate.
This review is about item#6563566.
Netting
5
From Japan
On 2018-08-24 13:07:04
I was anxious because it was cheap, but I can get at all normal.
This review is about item#6563566.
It is used to stop the messenger wire.
5
From Japan
On 2017-09-13 17:16:24
I often see M volts, but I think that 3/8 volts is not quite at this price. I am very satisfied. It is not convinced that it does not belong to bolts kindly.
This review is about item#6563566.
Banner fixing
5
From Japan
On 2016-07-16 16:33:59
I bought it with a pipe holder so that the banner rope does not slide down. The price is reasonable and saved.
This review is about item#06563566.
During maintenance of equipment
3
From Japan
On 2016-06-14 07:11:45
Although there was no dissatisfaction in particular, since it was in a bag one by one, I thought that I had extra effort to open a bag when I used it.
This review is about item#06563566.
As a fastener for car interior
5
From Japan
On 2014-10-09 15:41:36
It is installed under the rear opening of the Suzuki / Jimny JB 23W and is used to fix the load with a net or a rubber string. (Two places, screw hole of the frame will come out when removing the cap.) Eye bolts of inch screws are saved because there was no stock in the home center in the neighborhood.
This review is about item#06564354.
Swing bracket
4
From Japan
On 2014-07-17 20:50:25
I can use it without problems.
This review is about item#06563566.
1
Customer Who Viewed This Item Also Viewed
Eye Bolt
Eye Bolt, Stainless Steel
Eyebolt, M Screw
Eye Bolt Whitworth, Iron
Eye Bolt, Iron Chromate
Eye Bolt
Eyebolt, Inch Screw
Eyebolt
Eyebolt
Eyebolts wit (stainless steel)
Uni Chromate Plated Eye Bolt
Stainless Aiborutobuneji
Steel Eye Bolts
WATERPROOF HINGES
Eyebolt