Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Metal Aspirator, Body Only

Metal Aspirator, Body Only
Sales Price: 38.99 SGD
Review Rating: 4.38
8 Customer Reviews
5 star 5
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
"Veranda Goya Research Institute Implements Method to Install Micro Bubble Generator in Bath for about 6,000 Yen"
5
From Japan
On 2019-04-12 01:06:15
I am very happy with the above HP as a reference. I use it every day.
This review is about item#02981447.
For microbubble generation
5
From Japan
On 2018-01-19 17:46:51
Place it in the middle of the bath shower hose, close the suction port in the side and the micro valve comes out of the shower. When you put a shower head in the bath and take out hot water, the hot water of the bath is cloudy with a bubble.
This review is about item#2981447.
Blood test
5
From Japan
On 2015-10-03 19:52:11
Anyway it's the best, there's only this for washing Melangyur
This review is about item#02981447.
Well water purification
5
From Japan
On 2014-06-19 18:21:52
Price is affordable and easy to use
This review is about item#02981447.
Aquarium fish aquarium air supply and water circulation
5
From Japan
On 2014-01-14 22:03:26
Used by connecting to submersible pump for aquarium tank or external filter pump 400 L / h, air is sufficient but water quantity decreases, so it seems good to reduce pump discharge. Air suction sound is equivalent, so I am using a silencer mash. I think that it is convenient if there is a bamboo shoot attached directly to the aspirator air hose which can be purchased for about 200 ~ 300 yen without industrial use.
This review is about item#02981447.
Overflow spouting in pump up of tropical fish tank
3
From Japan
On 2013-02-13 21:13:14
How to use Wrong trout ... ... Improve the water quality of the carnivorous tropical fish tank (Clear from the look!) Asian Arowana · Da Tenio etc. ancient carnivorous fish multiple battle of foods eat UP fine going down (floating in water) micro? Nano? There is also a bubble and it promotes growth? Although there was decrease in flow rate after installation and increase in squirting noise (noise), I think that fish are happy, but I will look at the situation a bit more
This review is about item#02981447.
Micro bubble bath, and shower, for generation
3
From Japan
On 2011-10-28 14:13:49
No matter how we adjust the combination of water pressure, water temperature, intake air quantity, like micro bubbles like white muddy can not be generated A relatively large size bubble, so-called millibables, occurs a lot! Some micro size may be included in it! Is it?
This review is about item#02981447.
Used attached to shower hose for generating micro bubbles
4
From Japan
On 2008-10-16 12:27:05
You can enjoy a shower with considerably small bubbles if you increase the amount of water to a certain extent You can considerably reduce the amount of water used Foam gently shampoo etc
This review is about item#02981447.
1
Customer Who Viewed This Item Also Viewed
Silicone Tube
Metal Aspirator Trap
All Teflon Aspirator
Polyethylene Aspirator Body Only
Multi-Connector
Accessories for Aspirator
Metal Water Aspirators
No water pump glass steel valve
Aspirator made of PP with a check valve
Glass aspirator