Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Plastic box

Plastic box
Sales Price: 16.99 SGD
Review Rating: 4.50
12 Customer Reviews
5 star 8
4 star 3
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Outdoor wiring
4
From Japan
On 2018-11-04 09:17:13
It is convenient as a transparent box with a breaker visible. However, as the rainproof effect seems to be low, consideration is required for the installation place of rain.
This review is about item#7388945.
For board mounting of power generation equipment
5
From Japan
On 2018-04-10 15:18:29
It is convenient if it is slightly larger, because the plate portion is smaller with respect to BOX
This review is about item#7388954.
Device power switch case
5
From Japan
On 2017-06-20 20:49:43
The door was clear and easy to see, it was light and easy to install.
This review is about item#7388954.
As a drip-proof case of thermostat with digital display
2
From Japan
On 2017-06-02 20:23:38
Since the size of the breaker is barely enough, there is not much versatility because it is only the installation of one piece of equipment. It is about when waterproof and dustproof to install so that you can see the equipment with digital display.
This review is about item#7388945.
Installation of 400 mm canna board motor overload prevention equipment
5
From Japan
On 2016-12-16 23:35:11
In using Omron · Motor Relay K2CM to prevent burnout of the motor, it was necessary to understand without setting the lid, such as setting condition such as time and settling current value and when tripping. It looked good for an expensive motor relay.
This review is about item#7389015.
Put the instrument on.
4
From Japan
On 2016-11-17 16:53:20
I wish I had something a little narrower, but it was too small for one size to get bigger. The price is satisfactory.
This review is about item#7388963.
Distribution work
5
From Japan
On 2016-09-25 02:45:04
It is a transparent lid, it also shows the inside, very good. It is even better if there are more screw holes.
This review is about item#07388954.
Control box for motor installed outdoors
5
From Japan
On 2015-04-05 18:01:19
It is wonderful because you can see the breaker condition even if you can not open the lid as the inside sees from the outside.
This review is about item#07388954.
For distribution board expansion
5
From Japan
On 2015-03-24 15:51:36
It is a wonderful item with the best price. I appreciate gratitude.
This review is about item#07388963.
Storage of things on site
4
From Japan
On 2015-01-30 13:47:23
It is user-friendly.
This review is about item#07389015.
For preventing the electric shock of the control panel
5
From Japan
On 2014-06-16 14:45:50
Since there is a grid line on the base, it is possible to shorten the installation time without scribing the installation position of the equipment in advance. Moreover, it was easy to drill in the line and the assembly work was easy.
This review is about item#07389024.
For circuit breakers
5
From Japan
On 2013-03-20 17:13:41
It is used in indoor humid place. I see the inside looks handy.
This review is about item#07388945.
1
Customer Who Viewed This Item Also Viewed
Plastic Box
PCH-C Plastic Box
Wall Box, No Roof, Horizontal Type
Wall Box With Roof, Horizontal Type
Plastic Box, Lid
Waterproof Plastic Box
Polycarbonate Box
Wall Box, No Roof, Vertical Type
Without plastic box roof
Open/Close Plastic Box
Plastic box
KWH type makeup box
Free Plastic Box
Plastic box
Wall Box With Roof, Vertical Type
PBO type plastic box Outdoor rain-proof type
Plastic box
Free Plastic Box