Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Plastic box

Plastic box
Sales Price: 17.99 SGD
Review Rating: 4.29
17 Customer Reviews
5 star 12
4 star 2
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 17 of 17 Reviews
機械改造
3
From Japan
On 2019-01-22 10:16:38
いろいろな製品を確認し、コスト的に良かったので購入問題なく使用出来ています。
This review is about item#7388972.
Control panel production
1
From Japan
On 2018-09-02 18:20:29
Careful attention is required for processing transparent covers. The whole surface cracked by drilling and discarded. It is not suitable for application to cover the cover.
Used in electrical construction.
5
From Japan
On 2018-07-24 15:34:58
Since contents are understood without opening the box, it is very convenient for maintenance at a later date.
This review is about item#7388981.
For maintenance of machine
5
From Japan
On 2018-06-29 17:28:48
Delivery was speedy. Also, it's good to buy, it's robust, reliable and easy to handle.
This review is about item#7388981.
Passenger car battery charger storage
5
From Japan
On 2018-01-26 15:53:28
Since the door is transparent, the indicator of the charger body can be confirmed. For fixing, two tie-wraps of 350 mm size were connected in two sets on one side, a total of four locations. The mounting hole machined in the case was well made and it was easy to fix it to the pillar of the garage. The color of the main part is also quite good, I think that it is very good without feeling cheapness (temporary feeling).
This review is about item#7388981.
As a container of equipment for environmental measurement
5
From Japan
On 2016-11-12 06:41:52
I used a measuring instrument for temperature control and used it so it was very easy to see
This review is about item#07388972.
Outdoor wiring
5
From Japan
On 2016-09-25 03:01:05
Because it has an eaves, it is safe for rain, very good.
This review is about item#07388981.
Place the outdoor outlet in a plastic box for outdoor installation.
5
From Japan
On 2016-04-03 21:45:33
I want space inside the box at the back of the wooden base in the box.
This review is about item#07389033.
It was used as its accommodation BOX for installing a clock in an outdoor park.
5
From Japan
On 2016-03-24 17:14:52
There was a need for centering out because the squares of the setting board inside were not right and left targets.
This review is about item#07389051.
Outdoor meter
5
From Japan
On 2016-02-04 15:30:02
good. It is easy to see.
This review is about item#07389051.
Electrical work
4
From Japan
On 2015-11-09 15:18:12
Since the opening and closing door is transparent, I think that it is good to see it.
This review is about item#07388981.
Used for storing equipment related to sunlight control
5
From Japan
On 2015-09-15 19:28:38
It is convenient for checking the internal meter etc.
This review is about item#07388997.
Inverter box
5
From Japan
On 2015-04-21 15:19:39
Easy to install, it is good to see the inside.
This review is about item#07388972.
Sunshade of agricultural thermostat Removed rain
4
From Japan
On 2015-02-09 00:00:53
It is convenient to be able to check the temperature from the outside because it can be attached to the support with a cable tie
This review is about item#07388981.
Used for outdoor controller storage
5
From Japan
On 2013-12-25 15:45:18
Since the door is transparent, the controller display value can be confirmed even in the state that the door can not be opened, and also the owner was well received.
This review is about item#07389051.
For power supply
1
From Japan
On 2013-09-18 08:31:00
When I opened the box, the plastic of the lid was cracked and missing. I used this time for hurry to use. There were no scratches on the cardboard etc.
This review is about item#07389051.
Electrical construction
5
From Japan
On 2013-02-15 19:35:57
It was used for electric construction inside the agricultural vinyl house. For the door or clear, the inside is clear and convenient.
This review is about item#07388972.
1
Customer Who Viewed This Item Also Viewed
Plastic Box
PCH-C Plastic Box
Wall Box, No Roof, Horizontal Type
Wall Box With Roof, Horizontal Type
Wall Box, No Roof, Vertical Type
Polycarbonate Box
Plastic Box, Lid
Waterproof Plastic Box
Plastic box
Free Plastic Box
PBO type plastic box Outdoor rain-proof type
KWH type makeup box
Free Plastic Box
Wall Box With Roof, Vertical Type
Without plastic box roof
Plastic box
Plastic box