Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Metal Casing

Metal Casing
Sales Price: 8.99 SGD
Review Rating: 3.17
6 Customer Reviews
5 star 1
4 star 1
3 star 2
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Insect breeding
5
From Japan
On 2017-01-30 09:07:20
Convenient because the top is a screw type lid, with a hook on the back and can be hooked
This review is about item#7653204.
Used as protective tube at thermometer side
3
From Japan
On 2016-08-04 09:50:21
There was no fracture material when inserting the thermometer, there was anxiety of wire breaking contrary to rattling and I thought that it was kept as it was abandoned.
This review is about item#07653204.
Water temperature measurement
2
From Japan
On 2016-04-26 17:16:06
It easily breaks. Please be stronger.
This review is about item#07653195.
Temperature control of adhesive drying chamber
3
From Japan
On 2016-03-20 03:18:17
Purchased for Shimwa's thermometer. As was also the case with other reviews, the gap between the thermometer and the case is large, so the possibility that the thermometer and the case will be cracked as it is when dropped or the like is large, the scale is rotated and the scale is difficult to see. (I dropped it is bad, but the thermometer actually broke.) Now I use the cushion material on my own. The only complaint is that if you sell it with a cushioning material between the thermometer and the case. I am satisfied normally as a case.
This review is about item#07653195.
Measure air temperature / snow temperature to select ski wax.
4
From Japan
On 2016-02-04 21:36:06
Products dedicated to skiing are expensive, so we bought a thermometer and case separately. Although it was a product of the same company, I thought that it was useless because general versatility was necessary, but I thought that the gap between the thermometer and the case was large. (We fixed it using packing material of thermometer.)
This review is about item#07653204.
Protection of Shimwa rod thermometer
2
From Japan
On 2013-12-16 23:40:34
I bought it for the protection of Shimwa rod thermometer (30 cm), but there is sometimes a big play and the thermometer moves up and down or turns round. At the time of high temperature measurement, the bar glass expanded, so I thought whether there was play, but it was too big. However, the thermal expansion coefficient of this brass case is much larger than that of glass, so even if the size is properly adjusted, the thermometer will not be damaged. I do not know the reason why it is not fitting despite genuine products.
This review is about item#07653195.
1
Customer Who Viewed This Item Also Viewed
Bar Thermometer
Bar Thermometer
Simple Thermometer, Stick Type
Mercury Rod Shaped Thermometer
Portable Thermometer
Rod Shaped Thermometer
Mercury Thermometer
Liquid in Glass Bar Thermometer
Rod-shaped Thermometer Case
Glass Thermometer
Mercury Bar Thermometer