Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of AC Adaptor

AC Adaptor
Sales Price: -
Review Rating: 2.50
4 Customer Reviews
5 star 1
4 star 0
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
As an attached part of the company's products
5
From Japan
On 2016-01-14 16:25:40
I am sorry to hear that handling is over. There are people who have complaints, but this is not abnormal like this one. I am in trouble because of handling censoring. Would you please consider restarting?
This review is about item#08524302.
Industrial equipment
1
From Japan
On 2013-06-15 00:49:11
I bought a thing of 3V. I was out of 5.4 V when connected to equipment. I think that there are various ways to say that it is connected to the load. Even though there is no load even if it is normal it is a thing with specified voltage output ... It will not be usable at all. I would like to return the item. With this, Monotarou's trust will be gone. I thought that it would be better to stop trading.
This review is about item#08524275.
It is a general residential building and used to power the car drive recorder.
3
From Japan
On 2012-07-10 19:11:11
As the person who wrote earlier said, for DC12 I bought it was 18 V with tester no load. However, the live recorder I used was DC 12, DC 24, so it was not broken. It is operating normally.
This review is about item#08524311.
Used to power mobile PC.
1
From Japan
On 2011-07-21 18:46:13
When connecting to the mobile PC specified 9 VDC, the mobile PC became unusable in a few seconds after the screen was displayed. As the trial measured the output voltage of the AC adapter with the tester, it was 13.8 V, so it is natural that it is broken. Since there is a 12V specification in the lineup, it is probably a mislabeled label.
This review is about item#08524302.
1
Customer Who Viewed This Item Also Viewed
AC adapter 12W
AC POWER ADAPTER
AC adapter 20W
AC Adapter
AC Adapter UN Series
AC adapter UNL series
6V general-purpose adapter
AC adapter US series
AC adapter UU series
AC adapter UIA Series
AC Adapter
AC adapter 300
AC Adapter
Ac Adaptor