Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pack Roller R40

Pack Roller R40
Sales Price: 54.99 SGD
Review Rating: 2.83
6 Customer Reviews
5 star 1
4 star 2
3 star 0
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used for my own pizza dough forming machine
5
From Japan
On 2016-06-26 17:40:45
I made my own tool to extend the pizza dough. It is a mechanism to slide using two roller packs. I am happy to move smoothly.
This review is about item#09229227.
Camera slider
1
From Japan
On 2016-02-08 11:47:52
I bought it for movie shooting, but it did not move smoothly and it was not used at all. I think that there is no problem if it is used for slide rails such as drawers, but it is not good to use for taking pictures. Returns are also NG, so be careful who you are thinking for shooting.
This review is about item#09229166.
Light unit lateral movement device
4
From Japan
On 2015-10-09 09:04:07
I think that there is less play and I like places like bearings that can be used at reasonable prices instead of high price.
This review is about item#09229157.
Sliding door
1
From Japan
On 2015-05-08 09:26:58
Since you can not detach the hanging door after installing the slider in a place without stroke, I'd like to make improvements.
This review is about item#09229254.
Original camera slider
4
From Japan
On 2014-07-03 15:14:08
Since the commercially available camera slider is expensive from 1.5 to several ten thousand yen, we made a self-made camera slider with a tripod hole etc. based on this roller back as the base. If it is rigid and has a camera up to 2 kg, it made it move smoothly without problems. I was satisfied because I was able to do it at a fraction of the cost of commercial products. In addition, it was still better if the weight was a little more.
This review is about item#09229193.
I would like to use it for building furniture drawer, but is it applicable product?
2
From Japan
On 2009-04-11 15:16:07
It is a future story.
This review is about item#09229236.
1
Customer Who Viewed This Item Also Viewed
Pack Roller R25
Slide Pack FBW2560XR
Slide Pack FBW2560XR
Slider for R40
Slider for R25, Single
Slide Pack FBW3590XR
Joint Rail
Aluminum Slide Rail