Buy more than* S$200* and get FREE SHIPPING
Note
Due to Japanese national holidays, we will close 2018/12/29~2019/1/3 JST.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Shine Polish DC12V

Shine Polish DC12V
Sales Price: -
Review Rating: 4.80
10 Customer Reviews
5 star 9
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Vehicle polishing ~ Product polishing
5
From Japan
On 2015-10-05 16:26:21
It was nice to use easily. It is generally satisfactory because it is a polisher for power. I think that it is wonderful if it is possible to expand the range of possible work further if it is professional equipment.
This review is about item#09981395.
car wash
5
From Japan
On 2014-11-14 11:48:35
It's pretty good. Since I bought a 12 VDC type, it can be used at a charged car wash place etc. while putting on the engine. The sound is also relatively quiet and the plain water falls firmly. I think that this is sufficient for polishing private cars.
This review is about item#09981395.
easy
5
From Japan
On 2014-10-15 18:48:30
You can buy labor with cheap money
This review is about item#09981395.
Wax rush and window wipe up
5
From Japan
On 2014-10-12 20:36:12
It is satisfactory performance on the commodity, and after that I have to raise my skill. When liquid WAX was applied, the WAX ​​application time passed a certain amount, making it difficult to wipe properly accordingly. In the future, I thought that if I partially waxed it and let me wipe it off with my hands, the problem would be gone.
This review is about item#09981395.
Waxing
5
From Japan
On 2014-05-18 13:05:02
The sound is quiet and satisfying.
This review is about item#09981395.
I am using it for repairing the glass coating of my car
5
From Japan
On 2014-04-10 23:08:47
The feeling I used is a very good impression. It is also satisfactory because it is easy to make, and finishes cleanly from the application of coating agent to polishing without difficulty. As I had a lot of trouble manually, this is a good performance recommendation as well. I did not know until purchasing and seeing boxes and explanations, but it is a point that imported car is written as unusable. I do not know the reason for honesty. Is not it suitable for plating of cigar outlet? I was puzzled because I was an imported car. Well I think that I am going to use it as it is now because there is no abnormality that the main body and the plug gets hot, but if I knew it from the beginning it might not be purchasing. I hope you can display the information correctly and clearly.
This review is about item#09981395.
Waxing of cars and yellowing of headlights
5
From Japan
On 2014-02-14 16:03:52
The car wax stuck as if hung by hand, and it was applied irregularly in a short time. After, when used for yellowing of the headlights, as well as new, here is no longer uneven and I am really satisfied.
This review is about item#09981395.
Maintenance at the parking lot
3
From Japan
On 2013-08-09 21:32:39
For use in the parking lot of apartment, 12V specification is good. It's not as big as me. As expected the appearance etc. are suitable for the price, but it is not related to the work and consumables are also cheap so it will be able to use for a long time.
This review is about item#09981395.
For headlight polishing
5
From Japan
On 2013-07-13 14:42:05
I want a transparent feeling in the yellow headlight! Recently there are many such requests. Until now, I was doing a coating process by dropping it with chemicals. However, there are many scratches in polycarbona, we thought that polishing is the best, we bought this machine. (Sales maker is sold for wax of car body) ■ Prepared item ■ · Machine · Masking tape (Monotaro) · Blue Magic (Monotaro) · Homing Tough (for home kitchen) · Wet towel · Dry towel · Silicone coating agent or more Prepare and start work. ... As a result, scratches and scratches also disappeared, and Polka was more shiny than expected thanks to the hand polishing. It took about 30 minutes on one side for the necessary work in 10 minutes. The machine itself, somewhat bullable and the noise is also at a minimum level. As long as it is not midnight, you can use it in a condominium parking lot. It uses 5 A per hour due to power consumption of 12 V 60 W ... and so on. In my case, because of the polyka partner, the use time is short and the burden on the battery is hardly applied. I liked it because it can be used easily with a business trip service. The replacement puff is also inexpensive as a set of 3 pieces. The durability of this machine is unknown because it is used for the first time today. There is description of "one year warranty from sale date" in the instruction manual. I thought that it would be okay to have one for shorter working hours if I could take time to rub it.
This review is about item#09981395.
Car body maintenance
5
From Japan
On 2013-04-02 22:11:05
It is an amateur. I purchased this because there is no 100 V outlet nearby. I do not mind the sound. Rotation is not too fast, the main body is also light and usability is not bad. There is nothing short of power, for example, just stopping it against the car body will not stop. Although I used it for half a day, it seems that it does not eat electricity enough that the battery of the car goes up. Just think that there is enough room if the length of the code is a little more. Originally it is exclusively for waxing, but in my case I polished with a ground preparation called SULLRATAR'S SPIRIT before waxing. When I was polishing with my hands, I became sweaty and became Madara, which was serious, but it became firmly shiny and it was easy. I purchase separately sold puff set with this I think that 3000 yen free shipping fee is cheap. I'm satisfied with the correspondence of this store as soon as possible. It was a good product to say that it was good to buy.
This review is about item#09981395.
1
Customer Who Viewed This Item Also Viewed
Variable Speed Random Sander
Polisher Buff Set
Shine Polish AC100V
EP-300A Sponge Base Pad
EAP-245 Buff
Car Polisher
Sponge set for car polisher F-82