Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pressurized Ball Pen Air Press

Pressurized Ball Pen Air Press
Sales Price: -
Review Rating: 4.00
8 Customer Reviews
5 star 2
4 star 4
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Daily affairs
3
From Japan
On 2017-03-16 06:58:57
It is a regular pen, it is expensive as a ballpoint pen but the clip is sturdy and patronized to put it in the pants pocket, the short holding of ink is a drawback.
This review is about item#10064476.
Site
5
From Japan
On 2015-11-20 14:37:12
Even if you write in any direction ink will not be choppy. This is good! It is!
This review is about item#10064476.
As a portable writing instrument
5
From Japan
On 2014-12-20 00:13:30
There is a sense of security that you can put in any orientation, and it is used for portable use. Because it is short, putting it in your pocket does not get in the way. I also like the slightly thicker one.
Written in general
4
From Japan
On 2013-11-07 01:41:53
I could write it on damp cardboard. Sometimes the line becomes unexpectedly thick.
This review is about item#10064476.
Construction site
4
From Japan
On 2013-09-27 10:53:07
The overall length is shorter than usual and it does not disturb the work.
This review is about item#10064476.
Working note
4
From Japan
On 2013-08-28 22:34:05
Although it is somehow entered, it is the 4th one, but it does not protrude from the chest pocket, it is hard to fall even if it is clipped firmly and faces downward, fit is good! However, it is sometimes that knocks gather soon with fine powder and it becomes impossible to use it.
This review is about item#10064476.
Fill in the check sheet in the factory
3
From Japan
On 2013-07-12 13:06:47
It seems that the ink gets over. I think that it would be better if you can improve the overshoot of ink no matter how many times you knock.
This review is about item#10064476.
Outdoor memo writing
4
From Japan
On 2013-03-01 21:24:17
Dragonfly air press is good for portable use. However, it is unsuitable for desk work. It is shorter than the power tank, so it is not bulky with pockets, clips are solid and there are strap holes. Replacement core is also cheap. Power tank is too long for me. Since the core is commonly used with the product, it is supposed to be possible to handle four colors also unconfirmed. There is only 0.7 mm core, but a feeling like 1 mm. It is easy to get dirty with popping with the first touch since the ink is out too much. I think that if you have a 0.5 mm core you think that you can write fine memos and sketches nicely even outdoors, but I think that the shortcomings will also be improved. We also want to handle transparent models of air press and air press bouquets.
This review is about item#10064476.
1
Customer Who Viewed This Item Also Viewed
Uni Power Tank
Uni Power Tank Replacement Core
Ostwald viscometer
Ballpoint Pen
Pressurized ballpoint pen refill 1.0
SSJ stadium jumper
W-766 76 Stadium jumper black
Knock Ballpoint Pens