Buy more than* S$200* and get FREE SHIPPING

* Announcement of Payment Method Change *
Credit card payment is now available via Paypal platform.
Paypal account is not essential.
In addition to Visa and MasterCard, American Express, and Discover are also available now.
(Availability of each brand in your country follows PayPal policy)

Customer Reviews of LOF 45° x7° Offset Wrench

LOF 45° x7° Offset Wrench
Sales Price: 13.99 SGD
Review Rating: 4.00
4 Customer Reviews
5 star 2
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Work in a narrow area inside the car engine room
3
From Japan
On 2017-03-20 17:12:50
Even though the wedge wrench is 45 degrees, there is no way that it is left at 45 degrees. And also wrench of various angles. I wanted something like that, but it can not be helped. But, as it was lightweight and the hole was open, we wound a wire around it and worked while hanging it, and it was completed successfully.
This review is about item#10383615.
Used for car door change
5
From Japan
On 2014-04-21 13:22:14
Because the head was small, it was easy to access the narrow hinge part. I do not know the aggressiveness to screws, but there was not any slippage. I am worried that matte plating can not be removed.
This review is about item#10383633.
Maintenance
5
From Japan
On 2014-04-15 20:58:49
I bought this because I am missing scales with other goods so I purchased it as a purchase purpose but if I say the purpose of purchase and use, long (scale) and handling appearance are often scattered in work that requires urgent Even though it does not get in the way and it distinguishes designally from the point that it is distinguishable from the place I also tried to comment and I tried to comment It is convenient to use in combination with the company's product of the previous time But since the hand with two books is scattered, but
This review is about item#10383642.
Used for car maintenance
3
From Japan
On 2014-04-15 09:52:33
I used KTC for about 10 years and it is a replacement. We chose by amount, weight, JIS standard. I do not know until I use it for several years. I am worried whether matted paint (plating) will not come off. Should the screw slide, it should be replaced immediately.
This review is about item#10383651.
1
Customer Who Viewed This Item Also Viewed
Combination spanner
Double-ended spanner
LCWU Petit Combination Spanner
45deg x6 deg Long Offset Wrench
OF 45 degree Offset Wrench
Box End Wrench
Glasses wrench
Double Ended Glasses Wrench
Double-ended spanner
Master carbide bar for aluminum