Buy more than* S$200* and get FREE SHIPPING
---
*Notice*
Due to the maintenance, we will close our website from July 21,2018 10PM to July 22, 2018 4AM JST.
All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Resin Mirror Bracket, For Wall

Resin Mirror Bracket, For Wall
Sales Price: 30.99 SGD
Review Rating: 3.14
7 Customer Reviews
5 star 1
4 star 2
3 star 1
2 star 3
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Fixing the mirror when leaving the road
5
From Japan
On 2018-02-20 09:37:26
I can firmly fix the green onion, it is very good so there is no shake.
This review is about item#34913453.
I use it when I go out on the road.
4
From Japan
On 2018-01-23 16:13:31
I could fix it to the block, but it was a bit staggering.
This review is about item#34913453.
Installation of garage access mirror
4
From Japan
On 2017-11-13 16:12:57
There were not many things that could easily be mounted on the block, so it was a relatively easy-to-understand picture so I bought it. I would like you to post a picture of the back of the package so that you can see more of the screwdone's actuality. It should be easy to understand what type of mirror you can install. Although I used it right now, I would like another piece of equipment (as if the walls do not hurt) in the contact with the fence.
This review is about item#34913453.
For confirmation at the parking lot
2
From Japan
On 2015-10-15 08:26:54
Because it is a low price, it will be such a thing, I want a little more sense. If you tighten up to install it on a pipe, the pipe will collapse and the mirror mounting bracket will move even after installation.
This review is about item#34913453.
When going out of the parking lot on the road
3
From Japan
On 2013-10-04 00:09:48
It began to look good. It's a bit scary ....
This review is about item#34913453.
Garage mirror installation
2
From Japan
On 2013-08-23 21:00:07
There was a note in the package that the item itself was not particularly problematic, but it could not be used for those with a roof-shaped block on the block fence. It is caution necessary because it is not reflected in the image at the time of purchase. Well, if you look at the shape well, you may be able to understand it, but I hope that the part that is involved in the installation restriction is clearly indicated as clear.
This review is about item#34913453.
Garage practical use
2
From Japan
On 2013-03-11 18:26:04
It can not be helped because it is inexpensive, but it looks rusty because it is not stain. In addition, it is fixed to the block with a clamp type but because it can be tightened only by the upper person, the lower side opens and if it says extremely it is in the letter of Ha ... In the case of a house it does not matter as it is a feeling of hanging.
This review is about item#34913453.
1
Customer Who Viewed This Item Also Viewed
Eye All Mirror
Garage Mirror
Garage mirror mounting bracket
Round Garage Mirror
Garage mirror fixing bracket
Scissors included Mounting bracket
Garage mirror / pole bracket
Garage mirror mounting pole
Curved Mirror Clamp
For garage mirror attachment block
Garage mirror angle
Garage Mirror
Mirror Mounting Bracket
Garage Mirror