Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Steel Plate

Stainless Steel Plate
Sales Price: 5.99 SGD
Review Rating: 4.46
13 Customer Reviews
5 star 9
4 star 3
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
Seal around piping when passing through wall
5
From Japan
On 2018-08-06 21:38:23
I am satisfied with the item.There is no connection to the phone so I can understand the flat ones at the time of packing from here but it was not useful as a result of the dimpling on the top due to various items on top How to countermeasures
This review is about item#35633674.
Maintenance of the motorcycle
4
From Japan
On 2018-04-07 05:25:04
Since my career has broken, I cut it and put it on a tape and trying to use it. I have not processed it yet, but I think that it is a good product because there is no problem with welding.
This review is about item#35633647.
Restoration of restaurant kitchen wall
5
From Japan
On 2017-09-14 21:31:16
Cutting process was easy and construction was easy. It is inexpensive, made from customers as well.
This review is about item#35633735.
machine
5
From Japan
On 2017-08-28 15:31:53
It is a repeat. We are using it for maintenance and maintenance of machinery. It is very easy to handle.
This review is about item#35633726.
Control evaporated metal in evaporation source during deposition operation.
5
From Japan
On 2017-07-03 14:43:46
Both size and thickness are reasonable and usage is extremely small, but there is no sense of overcrowding. It is easy to use because it meets the needs of just as needed when needed.
This review is about item#35633631.
I have not used it yet
1
From Japan
On 2017-05-18 17:31:20
Although the goods themselves are good things, I thought what you thought, to pack the luggage, was bent and entered. Also, there are dimples on goods and feeling bad. Because it is a flat plate, I want you to pack with more care.
This review is about item#35633631.
For cake production
5
From Japan
On 2016-12-13 08:56:09
Size It is easy to use thickness. I also want to use it!
This review is about item#35633665.
For work
4
From Japan
On 2015-07-15 15:21:06
I purchased the parts used for a motorcycle to make it by oneself. I think that it can be produced if it takes time to reach this thickness. Since it is before work, there are no comments on the item yet.
This review is about item#35633631.
Original construction material
5
From Japan
On 2014-05-27 16:29:56
I was saved because I got the desired thickness.
This review is about item#35633656.
Makeups around the kitchen
5
From Japan
On 2014-04-25 17:21:46
When installing a gas stove, it is necessary to consider both splash prevention of juice and heat radiation, so we purchased a stainless steel plate with, and used it cut. Even with a thickness of 0.5 mm, it was easy to cut with a gold-cut scissors, but it is necessary for skilled to cut a cut into a clean straight line.
This review is about item#35633631.
Soil scooping tool used in excavation work
5
From Japan
On 2014-04-11 19:44:41
I would like to use a thickness of 0.4 mm if possible, but because of ease of processing 0.3 mm thick was used but there is no problem.
We used folding process to the part where structure is prone to corrosion.
4
From Japan
On 2013-10-19 13:31:15
Because it is a place that is very corrosive easily, I used 1 mm thick stainless steel in consideration of strength etc, but was 0.5 mm enough? I think.
This review is about item#35633717.
Work switch fabrication
5
From Japan
On 2013-01-20 20:01:51
Currently it takes days to ship so it will be appreciated if you shorten it further. The product itself is satisfied as expected.
This review is about item#35633717.
1