Buy more than* S$200* and get FREE SHIPPING
Note
Due to Japanese national holidays as Golden Week, we will close 2019/4/27~2019/5/6 JST.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Post-Assembly Ornemental Railing Top Sleeve

Post-Assembly Ornemental Railing Top Sleeve
Sales Price: 8.89 SGD
Review Rating: 4.29
14 Customer Reviews
5 star 7
4 star 5
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 14 of 14 Reviews
Product power cord
2
From Japan
On 2018-12-20 18:37:17
We bought 500 items this time, but we could only produce 493 pieces, due to the shortage of 7 pieces. We replenished with other makers' hands on hand, but it may become a complaint because the form is different.
This review is about item#36557841.
Car Maintenance
5
From Japan
On 2018-10-25 20:37:22
This type is difficult to escape, so it does not matter because the basic male is used on the non-supplier side, but since it is covered and protected to a certain extent by any chance, by mere escape, we use this type for mental hygiene. Since the absolute safety is the basis of the wiring work basics.
This review is about item#36557832.
Used for wiring
5
From Japan
On 2018-02-15 14:38:15
Delivery is also early and once a month 7000 yen If there is purchase history it does not cost shipping, it is very convenient to purchase at low price
This review is about item#36557832.
It is easy to handle short wiring.
4
From Japan
On 2017-07-13 09:25:04
Well, the wiring is short ~ I do not have trouble. Because it is a sleeve that can be put in afterwards There is almost no thing to get out if you do a successful male and female bond, and insulation is also okay. Just a bit thick, I think whether the space is severe as the number increases.
This review is about item#36557841.
Automotive wiring processing
4
From Japan
On 2016-11-16 14:47:47
Since the Giboshi terminal itself is not strictly standardized, there are slight differences between sleeves and manufacturers as a matter of course. This item fits neatly, much less than what is commonly used in audio harnesses (wiring model by wiring type) etc that are on the market. There is naming after-in, but it is possible to reduce things that "getting ahead" like a conventional product will "hurt your fingertips". That much, I made it crispy.
This review is about item#36557832.
Car maintenance
4
From Japan
On 2016-11-03 01:03:32
It is incompatible with the first-come-first-served and slightly larger than the first-come-first one. Depending on how you use it may be faulty.
This review is about item#36557832.
For wiring work
5
From Japan
On 2016-10-03 16:57:49
Price is cheap and it is saved. This type was saved because it was quite difficult to handle even in retail stores.
This review is about item#36557841.
Connection of wires, extension, addition etc.
3
From Japan
On 2016-09-29 16:27:17
Although there is no problem in terms of use, if it is an image of a product description, it seems to be a clear color with transparency but since the item arrived is pretty milky without transparency, it is not so bad when connecting with another company's product of the same shape I do not need it and it looks crappy.
This review is about item#36557832.
Car navigation system
4
From Japan
On 2016-05-27 15:46:08
It is cheap.
This review is about item#36557841.
I always bought it.
5
From Japan
On 2015-08-03 10:17:40
I am satisfied with stable quality. I am wondering how long the light resistance is from now, but the appearance when it is brand new is beautiful. Although it will be postponed, if I forget about it first and then I use it as a late admission.
This review is about item#36557841.
Automotive electronics in general
5
From Japan
On 2015-01-11 12:52:22
I will always use it. Usually the price and quality of goods are good. However, for regret only this time, there is a feeling that it seems that it was dirty and yellowish in both the outer bag and the main body, and there were two hair in (completely sealed plastic bag) It is not so good I did not feel like it (with pictures). Even though I did not look at it, it was a very conspicuous state, so it seems like a glimpse of the day-to-day attitude of the producers, etc. It is a pity. Whether the production base has changed or not, I discarded it because it is disgusting with a big losing this time. I expect it to be a good thing next time.
This review is about item#36557841.
Automotive electrical equipment installation in general
5
From Japan
On 2014-12-09 13:30:17
Even before or afterwards OK. It is safe and difficult to escape, especially when using heavy line or W line, it can be added later and it is useful.
This review is about item#36557832.
Repair of old audio equipment
5
From Japan
On 2014-12-02 23:18:21
As usual it is necessary to wire the sleeve first so that you can not clean it in practice or if you mistakenly attach a terminal different from the sleeve or do it again, use this product such as curing with tape Then you do not need that work, there is no place to worry about and smooth goes back. Although I purchased it as a set of 100 pieces, it is going to be used soon because it got used to various kinds of equipment as workability improved.
This review is about item#36557832.
Used for maintenance of used cars sold at our company, and customer visiting customers
4
From Japan
On 2014-07-01 09:22:39
We use it together with conventional sleeve. In the following cases, the rear insertion sleeve is useful. 1. The existing sleeve is damaged, and it is not easy to cut the kiboshi and insert a new sleeve in order to repair it. 2. A thicker sleeve is adopted as genuine depending on the model, and when you want to avoid using the general sleeve when adding a new wiring, it floats only there and it becomes full load of backing up. 3. The wiring that can be machined is extremely short, and it is impossible to crimp Kiboshi when putting the sleeve first. 4. In case you forgotten to put a sleeve by mistake and caulked Kiboshi. (Although rarely)
This review is about item#36557832.
1
Customer Who Viewed This Item Also Viewed
Bullet Terminal Set
Fork Terminal, B Type
(4600) R. Shoe