Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of ARS20S Aluminum Slide Rail

ARS20S Aluminum Slide Rail
Sales Price: 16.99 SGD
Review Rating: 2.00
1 Customer Reviews
5 star 0
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Development of farm equipment
2
From Japan
On 2014-10-28 13:40:02
I am indebted to you. Although the mounting hole on the top surface is 4 mm, the size of the head does not fit into the hole on the bottom but seems to be M 3, but the height of the head is too shallow so that the groove in the middle of the slide is shallow so it can not be used. Insertion diameter of the mounting bolt was small and it was not usable. We slightly scraped the diameter of 41489874 and somehow installed a thin plate. There is a thin stuffing at the bolt insertion hole of the slide base, which is distorted and it was not originally caught, so it did not slip smoothly so it is corrected and used. It is good to be able to use lightly and inconspicuously
This review is about item#36702215.
1
Customer Who Viewed This Item Also Viewed
Slide Rail S270
Pack Roller R25
Aluminum Slide Rail
SEBS-15B miniature slide guide