Customer Reviews of Stainless Steel Safety Wire
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Used for wiring the motorcycle

From Japan
On 2017-10-30 20:10:53
I do not mind failing with large capacity.
It's so long I do not know how long it will take to run out so good!
This review is about item#36657914.
Motorcycle Maintenance

From Japan
On 2017-05-19 21:47:48
The grip of the motorcycle is used to prevent slippage. Wire thickness is just right and easy to use.
This review is about item#36657914.
Used for wireless antenna wire

From Japan
On 2017-01-13 20:54:22
I was very satisfied that the amount was large for the price. Quality is also not bad.
This review is about item#36657914.
Bicycle wiring

From Japan
On 2017-01-04 10:52:07
Especially using it without trouble. I think that I can not use it because it is large.
This review is about item#36657914.
Maintenance of various engines

From Japan
On 2016-08-29 22:00:15
It is bigger than I imagined in the image. It seems to take considerable to use up.
This review is about item#36657914.
It is quite good ♪

From Japan
On 2016-07-13 14:30:36
Although it will not be frayed as it is, it has a good appearance, I bought a resin bottle at a 100 yen shop and put it in it. Since it is a 0.6 mm line, double triple lines are also finished neatly. I am very satisfied. The 0.8 mm line is necessary even if it is double, and it may not finish beautifully if the force is relaxed, so at that point it was as we expected with the 0.6 mm line. I am very satisfied with the quality, so I'd like to repeat, but perhaps it will not run out even if I take a lifetime ww
This review is about item#36657914.
Auto Repair Service

From Japan
On 2015-04-20 10:42:45
It was a bit cheaper than other cheap tool shops.
This review is about item#36657914.
Motorcycle Wire Lock

From Japan
On 2015-04-06 08:17:12
There is no problem at all. I think that it is the best item of COSPA.
This review is about item#36657914.
Repair of agricultural engine

From Japan
On 2014-08-18 22:00:49
It was used for repairing the agricultural engine, and it was used for the climbing of the fuel tank and the fuel hose of the alimono. Both price qualities exceeded the expectation of "necessary and sufficient". I am satisfied.
This review is about item#36657914.
Motorcycle, wiring

From Japan
On 2014-07-24 16:55:32
It is soft and easy to use.
This review is about item#36657914.
work

From Japan
On 2013-10-03 14:46:36
There is no particular problem
This review is about item#36657914.
1
Customers Who Viewed This Item Also Bought