Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Internal Assembly

Internal Assembly
Sales Price: 64.99 SGD
Review Rating: 4.30
10 Customer Reviews
5 star 7
4 star 0
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Repair of interior 3 steps
3
From Japan
On 2018-09-12 07:42:40
I ordered to repair the interior gear. As a result, due to lack of survey here, we could not use it. In some of the interior gears around 1995, there are cases where the exit of the pin is opposite to that which is currently mainly distributed, there is no compatibility. It is not a cheap part, so please make sure before purchase.
This review is about item#36799734.
Electric bicycle repair
3
From Japan
On 2018-04-12 17:41:10
Used for Bridgestone bikke 2e. I was able to replace without problems.
This review is about item#36799734.
Bicycle Maintenance
5
From Japan
On 2017-05-08 17:00:30
I am now on dry grease view but this price very satisfied with this performance
This review is about item#36799734.
Bicycle repair
5
From Japan
On 2017-05-08 08:10:52
Although it took a while to replace the sprocket, the unit replacement work itself went smoothly.
This review is about item#36799734.
Replacement of front wheel drive assist bicycle rear wheel internal gear shift gear
5
From Japan
On 2016-08-18 01:48:41
A cord wraps around while running, the pin of the rear wheel interior transmission gear breaks, and it is replaced with an amateur. Examine the exchange method on the Internet and exchange without problems.
This review is about item#36799734.
Exchange whole
2
From Japan
On 2016-02-23 22:26:08
I purchased it without understanding the meaning of the normal type of the product name. As it is 10 mm short, the nut can not be used because it is short. Cause · Normal means the axial length 181.8 mm. Please be careful. The electric bicycle compatible type has thicknesses of 1 mm thick, and should be purchased after measuring the axis length of 191.8 mm. There are 3 kinds of shaft lengths in total, so there are 5 types in total so please check the current shaft length before you purchase it. On the official page, if there is a representation of Shimano small part model number, we think that the risk of purchasing the wrong one will decrease. Please consider Y33S98320 SG-3R45 / SG-3R40 internal set assembly (shaft length 191.8 mm) Please search with this
This review is about item#36799734.
Commuting bicycle
5
From Japan
On 2016-01-28 10:02:05
It was surprisingly easy to exchange. I was thinking about disposing of bicycles, but I am likely to ride for the time being. I am satisfied with this product.
This review is about item#36799725.
27 inch city cycle
5
From Japan
On 2015-08-27 10:10:46
I tried to grease up myself and failed to mount it. Although the nail disengaged from the spring, I could not return it, but purchased here. I was able to ride normally the next day. Grease was painted and it was ok without time and effort. I would like to purchase some kinds of sprockets that can be used for this product.
This review is about item#36799734.
Panasonic Electric Assist Interior 3-stage Transmission Replacement
5
From Japan
On 2014-04-04 04:46:50
It was easy to replace without any special tool. Just as a shift from the old transmission, it did not have a shift push bar, so I think that it is a part of the transmission as certainly attached.
This review is about item#36799734.
Replaced as it broke
5
From Japan
On 2014-01-29 22:55:01
Since it was an electric bicycle, it seems that power was also applied at the time of shifting and it was broken. I was puzzled because it was my first exchange, but for Shimano's parts I was saved because I just exchanged without doing anything. I want to repeat at next exchange.
This review is about item#36799734.
1
Customer Who Viewed This Item Also Viewed
Roller Brake Unit
Piano Touched Lever
Grip Shifter
Unit Rear Hub
Bell Crank Set
Aluminum Rim
Small gear (Kogiya)
Stainless Rim Set