Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Both Sides Eyelet Punch Pliers, Separate

Both Sides Eyelet Punch Pliers, Separate
Sales Price: 24.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Tent repair
5
From Japan
On 2018-12-20 14:41:42
It was easier to use than imagination, it was very easy to use. I will buy it next time as well.
This review is about item#37295526.
Used to add to the bleeding of eyelets
3
From Japan
On 2018-06-02 05:15:02
Although I was hoping for opening, pinching and tapping, I was expecting a simple operation, but when I used an iron hammer like other caulking machines the caulking was deformed and failed three times. Since it is a wood (rubber, plastic) hammer in the instructions, I managed to use it somehow. I think that the diameter of the convex type is small, so it seems that it can not be caulked equally even if the compression is strong. That crimp is weak, it is regrettable that the eyelet turns.
This review is about item#37295526.
For bird eye shooting of the bird 's net.
5
From Japan
On 2018-02-07 20:07:19
Because it is a product of Trusco, it can be used with confidence. It seems that it will not last long if you hit too hard. However, because it is a separate type, it is very good to be able to hit eyelets even in the middle of the net or tent fabric.
This review is about item#37295526.
Leisure seats and sunshade net eyelets
4
From Japan
On 2016-08-15 22:30:45
Because you can remove the male scalpel and make it independent, it is convenient because not only the edge of the sheet but also the center eyelet can be made.
This review is about item#37295501.
To use as a cover sheet on the existing seat Eyelet is required to fix position
4
From Japan
On 2015-04-13 09:13:39
There was a mistake for the first time, but I got used to it and the procedure improved. It's very convenient because you can place eyelets in the center of the sheet.
This review is about item#37295526.
Drilling and reinforcing sheets
5
From Japan
On 2014-10-16 00:24:45
Easily drilled, we could put on eyelets. It is necessary to buy rubber hammer at 100 yen shop · · · ·. It is good that you can attach eyelets to the place you like.
This review is about item#37295501.
Fasteners for the blackout
5
From Japan
On 2014-07-23 13:27:58
Firmly, fixed and well suited for use.
This review is about item#37295526.
1
Customer Who Viewed This Item Also Viewed
Double-Sided Eyelet Punch
12mm Eyelet Punch
Grommet Punch Set
5&7mm Eyelet Punch
8mm Eyelet Punch
Both Sides Eyelet
Double-Sided Eyelet For Cast Rod
Punch Unit
Eyelet Punch Set
Hatomepanchi 5 & 7mm
Hatomepanchi
Dedicated Hatomekoma