Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Simple Pulley, No Becket, Snatch Type

Simple Pulley, No Becket, Snatch Type
Sales Price: 43.99 SGD
Review Rating: 4.80
10 Customer Reviews
5 star 9
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Loading work of accessories
5
From Japan
On 2018-08-31 15:23:35
It is easy to use with stitching. I will come in handy. Compact and lightweight so storage is easy.
This review is about item#37136671.
For raising and lowering the instrument
5
From Japan
On 2017-12-01 18:23:38
I felt the wheel rotation was smooth and easy to use. I am satisfied with both the size and weight of the pulley.
This review is about item#37136653.
Lifting a package
5
From Japan
On 2017-10-17 10:22:41
You could buy the same brands cheaper than home centers.
This review is about item#37136671.
Used to hang bikes and snowplows
5
From Japan
On 2017-02-23 18:37:27
It is used for electric suspended pulleys, but it is easy to hang, double hang and detachable
This review is about item#37136671.
People's movement
5
From Japan
On 2016-12-09 14:00:12
Place a steel wire between trees and trees to make facilities for hanging people. I am worried that it will not rotate smoothly with the rust of the roller, but I think that it can be easily removed from the wire.
This review is about item#37136671.
maintenance
3
From Japan
On 2015-12-01 18:13:49
It was bigger than I expected. It can be used normally. A little more compact is better.
This review is about item#37136653.
Branch dropping of trees of Takagi
5
From Japan
On 2015-11-21 01:41:46
Lifter · Sky Master · Crane etc. place where heavy machinery can not enter, cut a branch hanging on the roof with a chain saw and let it down with 2 to 3 pulleys. It is more reliable than working with a tripod, if there is a lifeline. To excessively trust a tripod or a stepladder is dangerous.
This review is about item#37136671.
In the collecting work of shiitake mushroom tree
5
From Japan
On 2014-07-27 21:23:35
An angle is attached to a light tiger, and it is pulled to a loading platform with a 12V winch, but a simple snatch pulley is attached to the tip of the angle, and loading has been done efficiently.
This review is about item#37136671.
For experiment
5
From Japan
On 2013-08-30 16:06:24
I was searching for a small and firm snatch type, but this was also the best for cost. It was also easy to open and close, so it was hard to come off and it was safe to use it.
This review is about item#37136671.
Intermediate logging of standing trees
5
From Japan
On 2013-03-21 12:45:14
Even if the end of the rope is enlarged, you can set the rope even from the middle of the rope, small size and good workability. If you want greedy hook rope may be a bit shorter to prevent sticking. If so, multiple ropes are safe when they set no longer hitting this metal fitting.
This review is about item#37136671.
1
Customer Who Viewed This Item Also Viewed
Simple Type Pulley, Shackle Type
Simple Iron Pulley Hook Type 50mm
75 mm bearing pulley
Single Pulley, Tie
Simple yer Funding hook type bearing input
Saury block (Ofu type)
Simple iron block hook type bearing input
Simple snatch hook type 2 car
Simple snatch hook type bearing input
Rope hoist
Yeah Funding block shackle type