Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Confit

Confit
Sales Price: 12.99 SGD
Review Rating: 4.29
7 Customer Reviews
5 star 3
4 star 3
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Renovation
3
From Japan
On 2015-10-22 11:42:51
I would like to purchase again if I have the opportunity.
This review is about item#38565852.
Used for structural plywood 12 mm
5
From Japan
On 2014-12-20 01:20:34
Because it will tighten up strength is easy to put out! Working efficiency is good because there are few scratches! It is!
This review is about item#38565861.
Floor dowel operation
4
From Japan
On 2014-11-14 19:47:12
There is a thing in which there is not properly formed the plus part of one or two heads in one box, and there is a case that a plus driver does not enter.
This review is about item#38565852.
Attaching a control panel
5
From Japan
On 2014-04-30 07:32:43
The degree of tightness with ordinary screws is totally different. This can be used with confidence. Thank you.
This review is about item#38565861.
Tightening of under plywood plywood
4
From Japan
On 2013-12-11 09:23:52
Since the flange is attached to the head, tightening of plywood and joist is much different. In addition, it is unnecessary to do postprocessing because it is difficult for sasakule to come out.
This review is about item#38565861.
Effect on floor sounding
4
From Japan
On 2013-11-28 05:44:32
I bought it for repairing the flooring of my room. I struck it from above the joist which is close to the place where it is ringing but it seems that both the real ringing and the floating floor have almost been repaired. It was good that there were a small amount of goods for individuals because they used only 4 in 500 bottles and had a large amount of surplus.
This review is about item#38565861.
Floor construction
5
From Japan
On 2013-04-29 21:18:17
The neck under screw seems to firmly support the upper material and prevent floor squealing. Surely the tightening force is outstanding.
This review is about item#38565861.
1
Customer Who Viewed This Item Also Viewed
Plywood Screw
End Check Prevention Screw
Compagnis Parker
Konpanebisu Disugo
confit
  • confit
  • East Japan Power Fastening Co.,Ltd.
  • 4.99 SGD
  • 5.000000(1)
Compainvis (small box)
Bearing wall bis
Nedanotto (iron / Dacro) (small box)