Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Steam Humidifier

Steam Humidifier
Sales Price: 359.99 SGD
Review Rating: 3.80
5 Customer Reviews
5 star 1
4 star 2
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Humidification of office
3
From Japan
On 2017-12-28 15:17:32
It is very regrettable that there was a place not displaying one place in the part where digital humidity is displayed, but since it does not interfere with the function, it is used as it is. The amount of humidification is sufficient and satisfactory. The sound of the fan is no problem in the noise of the office level at all.
This review is about item#39115571.
Working at the factory
4
From Japan
On 2017-12-28 14:55:27
I am a little more late that water decreases a little more. It is troublesome to add water.
This review is about item#39115571.
Flooring 20 tatami mat 2F Used for stairwell
3
From Japan
On 2017-02-23 08:53:27
Although it is the third year (winter only) after purchase, as impressions used, humidification power is enough. Easy water supply once a day (weak driving 12h - 16h). However, frequently (if you use it every day, at least once a week) it is difficult to take this because it will crystallize on the evaporating dish unless you clean it internally. Even when cleaning the interior, it is very inconvenient and exhausting because it is necessary to wash a very heavy body entirely, such as in a bathroom. Since the inside of the periphery other than the evaporating dish also becomes dirty with a light brown color, it is rubbed with a soft brush or the like, but some parts can not be cleaned well by the structure. I wish I could disassemble a little more. Also, with daily water supply, the upper lid when removing the tank and a lot of water droplets are attached to the tank itself, and when water is supplied, the pots and water drips to the floor. Although the tank is also a poly container, it is pretty dangerous because the sharp edge is pretty well formed. Although improvement points are many, I think that it is excellent with cost and humidification power.
This review is about item#39115571.
Moist inside the office
5
From Japan
On 2017-02-02 09:08:59
Humidification can be done faster than other companies' things, but I think that the sound is somewhat larger
This review is about item#39115571.
Used in office with 20 tatami mats with colonnade
4
From Japan
On 2016-01-14 15:59:29
I use the water tank for about 10 to 12 hours for a whole day with full tank, but it is easy to finish with water once a day. I think that it may be better to have more humidification power because it uses a large heating for rebar building. Cleaning is easy.
This review is about item#39115571.
1
Customer Who Viewed This Item Also Viewed
Filter set for SFH-12
Powerful hybrid humidifier
Hybrid humidifier