Customer Reviews of Tap Holder
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Screw repair work

From Japan
On 2017-11-22 21:29:02
I went out because the size I wanted was out. I was able to finish the work with a good touch.
This review is about item#19327035.
Re-tap paint clogged nut

From Japan
On 2017-05-26 23:23:17
Since the tap is locked, work can be done quickly because it can work continuously.
This review is about item#39411461.
Threading by tapping

From Japan
On 2016-02-04 21:15:18
Even if you install a tap and turn it with a ratchet handle It is also good to install it on an electric screwdriver Allowing thread cutting earlier than conventional tap handle is convenient. I recommend you to size all sizes of thickness.
This review is about item#39411407.
Car maintenance

From Japan
On 2015-06-19 17:30:27
There is no problem with car maintenance
This review is about item#39411391.
For work

From Japan
On 2015-04-30 22:42:37
I used a 1/4 plug-in tap holder in my workplace. When I was using it, I used it as it should be, but when I used an ordinary tap holder - I felt that the fixed part loosened and it was hard to use. Actually 1/4 was good, but since I do not seem to be currently on sale, I purchased this item. I think that the usability is good. However, when used with a 3/8 handle, the force is overloaded and it seems to break. I converted it to 1/4 and use it.
This review is about item#39411425.
Tap processing Used with rechargeable drill

From Japan
On 2015-04-20 09:34:10
It is very easy to detach the tap. Tap It is easy to use with torque adjustment with a rechargeable drill that can be fixed without slipping
This review is about item#39411391.
For re-tapping

From Japan
On 2015-03-24 20:03:37
I used it on my ratchet. Because it was a small place I found this item where I was in trouble because I could not normally use the tap handle. Tap never escaped, we could work with confidence.
This review is about item#39411461.
Aerial work

From Japan
On 2014-06-03 13:15:52
Very good. I also proceeded to work colleagues and bought some pieces.
This review is about item#39411407.
1
Customers Who Viewed This Item Also Bought
<<
>>