Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Steel Latch

Stainless Steel Latch
Sales Price: 5.99 SGD
Review Rating: 2.50
2 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Temporary connection between wood
4
From Japan
On 2017-06-07 22:19:54
There was nothing like being improved only by the top one point as others wrote in the review, or it is fixed securely with two points. Pins are made so that they can not be removed, so there is no need to worry about losing them. In addition, it is hard to understand in the photograph, but also fine parts are satisfied, such as pin parts are processed so that fingers are easy to get caught when unlocking.
This review is about item#39454466.
Very weak
1
From Japan
On 2015-08-24 14:14:59
I do not know if you see it in the image, but this hinge is not stopping at the lower part. In other words, the hole at the bottom of the image is a waste of all, the problem which is only decoration, the hinge only remains at one point above That's because commercially available hinges are supposed to stay at two points at the top and bottom, not to mention it goes without saying that there is a strong anxiety at a single point. In this case it will easily get twisted with the force to open the door
This review is about item#39454475.
1
Customer Who Viewed This Item Also Viewed
Hinge Hook
(17858) Hose, turbo-to-oil cooler
Steel Roller Catches
Hinge premium
RESIN PULLS
No410 handle
Hinge premium
Sten hinge premium
Strong premium