Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of goot Quick Heat Soldering Iron

goot Quick Heat Soldering Iron
Sales Price: 40.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Part installation and removal
5
From Japan
On 2017-07-11 16:57:39
Because it is a gun type it is easy to hold and easy to work. Heat transmission is also fast, which has led to increased work efficiency
This review is about item#39528623.
When producing tube AUDIO
5
From Japan
On 2017-06-22 06:52:43
Until now soldering wiring work, I used ANTEX made solder iron of 18 W but by all means the heat capacity is insufficient at the terminal of the power transformer, around the earth, unless another 100 W, 200 W iron is used, if it is not workable had. In such a case, just by pushing SW, the heat capacity is up, I like working a lot and I love it a lot.
This review is about item#39528623.
Soldering parts and removing soldered parts
5
From Japan
On 2014-10-23 22:45:34
The soldering iron tip of TQ - 65 which I used so far has broken, it seems that there is no change of soldering iron tip, so I updated it to TQ - 77. ① The startup from switch-on is fast, and it can be cleared up as soon as it is finished, so the entire work ends quickly. ② Because the high power switch is in the handgrip, soldering with high power can be done easily.
This review is about item#39528623.
Regular soldering operation
5
From Japan
On 2013-08-08 22:43:39
I bought the same good quick heat soldering iron TQ - 80 twenty years ago, but this model was supposed to purchase this TQ - 77 as an additional purchase because it is hard to push a quick heating button a little. I think that it can be used for a long time as TQ - 80 has been used for many years. Button is also easy to push easily. However, MonotaRO is not cheap except homemade. If this product alone, it was 700 yen higher than the cheapest price of other shops, but there were other items to buy and coupons could also be used, so considering including shipping costs became cheaper than buying at other stores separately I bought it with MonotaRO. There are other things that I would like to purchase, but if it is about 8 thousand yen, I would like you to work hard so that you can offer cheaper than many other stores even if you use coupons.
This review is about item#39528623.
1