Buy more than* S$200* and get FREE SHIPPING
Due to the new coronavirus, there has been a surge in demand for safety protective equipment such as masks and protective clothing and therefore, production is not meeting the demand currently.
Some of our products are out of stock and it is difficult to accept orders.
We apologise for the inconvenience caused to you.
We sincerely ask for your kind understanding.

Customer Reviews of ESLON Heat Insulation Tube LTQ

ESLON Heat Insulation Tube LTQ
Sales Price: 9.99 SGD
Review Rating: 4.61
18 Customer Reviews
5 star 12
4 star 5
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 18 of 18 Reviews
Insulation of hot water supply pipe
5
From Japan
On 2019-12-29 19:36:34
The one that had been wound up now became old and cracked on the surface, so it was replaced. It was attached very easily because there is a tape.
This review is about item#39540907.
Air conditioning piping insulation work
5
From Japan
On 2019-10-23 22:11:28
It was flexible and had heat retention, making it ideal for preventing condensation on piping.
This review is about item#39540952.
Insulation of outdoor water supply pipe
4
From Japan
On 2018-11-29 17:30:02
Easy to cut and easy to install because it has a tape.
This review is about item#39540952.
Used for machine maintenance
4
From Japan
On 2018-09-03 21:21:11
The straight piping was very easy to cover, but it is hard to bend because it is hard except where it curves a little.
This review is about item#39540925.
It is used to keep piping warm.
5
From Japan
On 2018-04-23 19:37:10
The tape was slightly peeled off. Otherwise no particular problem
This review is about item#39540916.
To the piping of the car air conditioner
5
From Japan
On 2018-04-04 05:06:54
When I used it for heat insulation of a car air conditioner in a magazine, since there was an article which became cooler well, I wrapped it experimentally. Since the vinyl on the surface will blaze with the heat of the exhaust, if you wrap the heat shield of glass wool further, it will have an effect, it will cool down cold. Moe, the best.
This review is about item#39540891.
To keep the piping of Eco Cute warm
5
From Japan
On 2018-01-18 14:39:59
About 10 meters of bath and Eco Cute tank The inside of the pipe was cold and cold water went out Just winding this, I am surprised by the feeling Differences that made it hard to chill appeared It is easy to handle and satisfying even if you use it.
This review is about item#39540934.
Water pipe heat retention
5
From Japan
On 2016-04-10 17:04:05
It was saved.
This review is about item#39540916.
Protection of hot water piping (prevention of burns)
3
From Japan
On 2016-04-02 19:35:02
The straight tube part is also clean and the finish can be used without problems. Elbow part cut to 45 ℃ and inherited a gap, I really want a type exclusively for elbows. It is saved if there are tapes that fill the clearance.
This review is about item#39540934.
Prevent freezing of Eco Cute resin piping
4
From Japan
On 2016-02-08 22:26:47
Since the insulation material of the frozen resin piping was deteriorated, it was installed to prevent freezing. Construction was very easy, but it was a thick insulation material so it seems that it became a pipe with the thickness of the previous twice.
This review is about item#39540891.
Homebrew solar water heater piping heat retention
5
From Japan
On 2016-01-16 09:22:12
It was cheap and sticky, and it was easy to work.
This review is about item#39540891.
Air conditioning construction
5
From Japan
On 2016-01-14 19:58:59
Polyethylene foam has high insulation effect as it does not scratch. Adhesive tape firmly attached.
This review is about item#39540916.
Hot water supply equipment piping
5
From Japan
On 2015-11-25 18:18:30
Easy to handle
This review is about item#39540916.
Hot water piping heat retention
4
From Japan
On 2015-08-17 15:58:55
There is no problem with the straight part, but the bent part wanted a dedicated part.
This review is about item#11760236.
For home air conditioning piping repair
4
From Japan
On 2015-07-16 22:32:48
The heat insulating material which covered the air conditioning piping deteriorated and the cooling efficiency was lowered, so it was removed and replaced with this one. It is difficult to wrap up in a sudden R place, but it can not be helped thought from the insulation of the heat insulation material. The material of the surface was a solid material and it seemed to be able to withstand ultraviolet light for a while for a while. I think that it is very convenient and good for the linear part.
Heat preservation for energy conservation
5
From Japan
On 2014-02-12 20:29:51
It was easy to cut with a cutter knife and easy to use.
This review is about item#39540907.
Water heater bait protection
5
From Japan
On 2014-01-30 13:15:30
Because it was a one side seal, installation was easy. I feel that the material is also hard to deteriorate.
Pump piping heat retention
5
From Japan
On 2013-11-17 18:45:29
Easy to use but color was cream.
This review is about item#39540943.
1