Customer Reviews of LEGETOLEX

LEGETOLEX
Sales Price: 27.99 SGD
Review Rating: 4.71
17 Customer Reviews
5 star 13
4 star 3
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 17 of 17 Reviews
As a DIY
5
From Japan
On 2018-12-12 19:45:51
There was more soundproofing than I thought! I would like to construct it elsewhere.
This review is about item#39541941.
Quietness of the dishwasher
3
From Japan
On 2018-11-23 15:42:06
I bought it because I care about the sound of household dishwashers I bought two pieces, one on the back side, the second one cut in half and stuck to the left and right. I do not measure the sound pressure so I can not say exactly but I think it has become somewhat smaller
This review is about item#39541941.
Vibration reduction of mini vehicles
5
From Japan
On 2018-07-21 08:39:06
It was effective. The arrival of goods was relatively fast, and the packaging was solid.
This review is about item#39541941.
Detroit of trunk room
4
From Japan
On 2018-03-24 00:33:56
I used it for the trunk room of the Roadster. Although it was easy for processing, it was a beginner, but the finished level was satisfactory. Although there is no dramatic change as an effect, I feel Mima's silence effect. Smooth delivery was saved.
This review is about item#39541941.
Prevention of abnormal noise
4
From Japan
On 2017-12-20 08:22:20
As I have used before, I also purchased because it is easy to use because it is large in size and easy to use.
This review is about item#39541941.
Automotive deadening
5
From Japan
On 2017-10-16 14:47:35
There are many similar products, but overwhelmingly superior in terms of ease of construction and price.
This review is about item#39541941.
Car maintenance
5
From Japan
On 2017-09-20 18:56:38
The price was attractive and I bought it. I am satisfied with great success in car maintenance.
This review is about item#39541941.
For vibration damping of passenger cars
5
From Japan
On 2016-07-16 00:33:53
Although it is used for deadening of passenger cars, it can be used with confidence.
This review is about item#39541941.
Vibration control of car
5
From Japan
On 2016-05-24 09:33:54
In order to reduce the road noise of the car, we first tried to stick it inside the tire house and outside the fender liner. The noise of the road surface called "go" changed to a low sound quality that was felt as a go, and the volume was also reduced, so there was an effect. Because there is adhesive strength, it was attached with a simple cleaning of the degree of water wiping firmly. It also holds down the entire board surface firmly so as to correspond to fine asperities as well. By the way, the same product was sold also in the home center in the neighborhood. For those who want to use in large quantities, let's investigate those with an area of ​​1/4 size at about 1.5 times the amount. Monotaro san, it is recommended.
This review is about item#39541941.
Reducing wind noise of the hood on the outer wall of the house
5
From Japan
On 2016-01-27 15:44:40
Because the rain sound of the hood of the 24-hour ventilation opening in the residential bedroom and the wind noise were amazing, it was lining the inside of the hood Effects I was sickened
This review is about item#39541941.
Vibration control of car · silent
5
From Japan
On 2015-12-06 23:32:56
We performed the entire surface inside the door outer panel and inside the floor panel. Shearing It is easy to adjust the size appropriately according to the place of use. There is no peeling even with good adhesion and without degreasing. Because it is flexible, it can be applied neatly to irregular surfaces. Although it is the important vibration damping and silent sound, this has individual differences (subjectivity) but apparently it is not comparable to before construction. (For example, a mini car with an iron plate burned out would be about the same as the quietness of a luxury passenger car class if it says in the meantime.) Incidentally, this time it took effect on a light wagon car, but we used 8 cards. Even if you do not use any other soundproofing materials or other like this, you will not mind vibrations or external noises.
This review is about item#39541941.
Damping material of car body
5
From Japan
On 2015-05-07 15:17:25
I put it on the luggage, but I think that it is lightweight when using it over a wide range. I think that I will also use it for damping the roof.
This review is about item#39541941.
Car repair
4
From Japan
On 2015-04-15 20:01:29
Good
This review is about item#39541941.
Sound insulation
5
From Japan
On 2014-10-07 23:00:42
There is considerable effect. The sound has run out.
This review is about item#39541941.
Car Detaining
5
From Japan
On 2014-05-23 15:47:22
I wish it had a slightly bigger size
This review is about item#39541941.
To reduce the noise of private cars
5
From Japan
On 2014-04-21 20:34:29
Suitable for cutting
This review is about item#39541941.
Car noise reduction
5
From Japan
On 2013-10-27 09:05:34
This is fine. If it is a little vibration you can use the chatter sound inside the car. Recommended.
This review is about item#39541941.
1
Customer Who Viewed This Item Also Viewed
Sound Absorbing Sheet
Sound Insulation Sheet
Sound Absorbing Material, Floor
Insulation Sheet
Engine Room Sound Insulation
Road Noise Reduction Mat L
Sound Deadener
Calmflex,with Adhesive
Deadening Kit
Vibration Damping Tape