Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of TPX Check Valve

TPX Check Valve
Sales Price: 34.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 2
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I used it as a check valve
5
From Japan
On 2018-06-12 09:08:46
I think that it is a good thing that was useful for purpose because it prevents reflux and reflux I use it to prevent reverse charges when appendix from tank
This review is about item#58107445.
Aeration to culture medium
4
From Japan
On 2017-06-19 01:46:24
It is convenient because autoclave is possible. If the water pressure is strong, it seems to hold back flow considerably firmly, but if there is no pressure more than a certain level liquid will leak little by little. It is not suitable when you want to prevent water leakage with weak pressure.
This review is about item#58107436.
To check the water
4
From Japan
On 2016-10-15 17:20:27
I connected it with a silicon tube with an inner diameter of 5 mm, but cut it and use it with a smaller tip diameter to increase efficiency. You can use it with a good feeling. It is not 6 packs, it is enough for single item or 2 packs.
This review is about item#58107427.
Prevention of sagging of liquid sparging device
3
From Japan
On 2016-03-14 21:18:54
I put a spring inside and made it work even if I lie down. It is a schedule.
This review is about item#58107427.
I used it as a crank internal pressure control valve of a motorcycle
5
From Japan
On 2013-10-18 18:42:23
I am satisfied that the emblem is mild. It is transparent and easy to maintain, and it is safe because it can be used for a while because it has 6 items in it!
This review is about item#58107445.
1
Customer Who Viewed This Item Also Viewed
Mini Luer Fitting
Check Valve
Backflow Check Valve
Check Valve
Check Valve Polyacetal
One Way Valve Ball Type
Tube Check Valve
Check Valve,
Check valve set
PTFE check valve
Check Valve
Diaphragm check valve
Check Valve, PE