Buy more than* S$200* and get FREE SHIPPING

* Announcement of Payment Method Change *
Credit card payment is now available via Paypal platform.
Paypal account is not essential.
In addition to Visa and MasterCard, American Express, and Discover are also available now.
(Availability of each brand in your country follows PayPal policy)

Customer Reviews of Bifocal Reading Glasses RB-1

Bifocal Reading Glasses RB-1
Sales Price: 25.99 SGD
Review Rating: 3.70
40 Customer Reviews
5 star 16
4 star 10
3 star 4
2 star 6
1 star 4
The reviews are automatic translation.
Showing 1 - 20 of 40 Reviews
Used for normal use.
5
From Japan
On 2019-06-17 15:31:16
The wide naked eye part is wide field of view, the presbyopia is under, and besides the work, it is satisfactory to think from the price, adapting to fine work such as fishing tackle.
This review is about item#59031253.
Pump core and protective glasses
5
From Japan
On 2019-04-30 15:33:08
Since the workplace is using medicine, I use it one 2 2 other roles conveniently without replacement.
This review is about item#59031262.
Welding marks and cutting spatter removal
3
From Japan
On 2019-04-10 23:07:25
Is the reading glasses part a magnifying glass? I feel uncomfortable because I get bigger when I enter the presbyopia lens part. However, it may be good to see the scale and so on.
This review is about item#59031253.
Metal processing
5
From Japan
On 2019-04-02 16:43:54
Protective glasses and reading glasses are saved as one. You can not give up while working because metal fire powder does not damage expensive spectacle lenses.
This review is about item#59031271.
for work
4
From Japan
On 2019-02-01 21:23:46
The percentage of reading glasses was the best percentage for me over what I used before.
This review is about item#59031262.
Used when looking at detailed letters such as manuals
1
From Japan
On 2019-02-01 15:31:45
The part of the reading glasses is too low to use. Seeing other people's reviews, it seems to be relatively satisfying, but I can not use it. If the upper part, the part of the reading glasses is a little more wide, it may have been usable. To me, it became an unusable item.
This review is about item#59031262.
Earth work
5
From Japan
On 2018-12-24 20:06:32
I was looking for this glasses. It is saved when far-field work comes out frequently.
This review is about item#59031253.
Wear when bike commuting
5
From Japan
On 2018-11-08 11:40:59
Purchased for the purpose of guarding the eyes from pollen and dust at bicycle commute. As mentioned elsewhere, the reading glasses part is narrow at the bottom and the boundary is also conspicuous, but the display of the hand clock or the cycle computer is well visible, and the fact that the part with no degree is wide is aided conversely. I will purchase additional.
This review is about item#59031253.
Detailed work
2
From Japan
On 2018-09-02 23:39:13
The part of the magnifying glass is still small. I have a bit of a nose rash. I feel heavier than before.
This review is about item#59031271.
Used when entering personal computer
2
From Japan
On 2018-06-11 17:19:36
Only one point is dissatisfied. "Reading glasses part does not enter sight! " Reading glasses lens is too low to go into sight. It is useless as reading glasses. Other than that, there are no particular problems, so it is a more disappointing item.
See fine sentences
5
From Japan
On 2018-05-24 18:12:11
I've tried taking prescription eyeglasses with presbyopic eyes so far that I can see the characters I could not see anywhere.
This review is about item#59031253.
Instrument measurement
4
From Japan
On 2018-04-26 06:26:01
While working, I use a caliper depth dial gauge Before purchasing I attached 1.5 times the lens to ordinary protective glasses Purchased here with a trouble, surely the lens position is too low I will get used to it.
This review is about item#59031253.
During carpentry work
1
From Japan
On 2018-04-13 21:30:55
Reading glasses are hard to see even if the parts that look like reading glasses are too low. I can not see it clearly. Reading glasses are not strange, but reading glasses are strange.
This review is about item#59031271.
When putting the material into the machine.
5
From Japan
On 2018-03-07 22:23:56
After putting in the material, when replacing the box containing the finished product, you do not have to take the glasses one by one as you read the counter figures.
This review is about item#59031262.
General work, Sports
5
From Japan
On 2018-01-26 09:21:37
It is very handy. Every time a scratch becomes conspicuous it is replacing the sixth machine. For sports such as cycling, running, it is best for measures against ultraviolet rays. I attach the pad because the lens is too low. Complaining dissatisfaction is possible if pad angle adjustment is possible.
This review is about item#59031253.
Used when working nearby
5
From Japan
On 2017-10-30 16:24:25
Both the nose pad and earpiece are soft and firmly support, so there is no misalignment and the feeling of use is good. Personally it is easier to use if the lens is a little bigger.
This review is about item#59031271.
Steel
5
From Japan
On 2017-10-10 18:48:49
It is very good to see small scales etc. It became indispensable to work.
This review is about item#59031271.
Inspection work
4
From Japan
On 2017-09-27 23:23:03
The reading glasses part is convenient when approaching by inspection work and checking the details.
This review is about item#59031262.
Carried for travel etc.
2
From Japan
On 2017-05-10 13:26:18
It is kind of annoying. The boundary between the lenses is unnatural and the eyes feel tired.
This review is about item#59031253.
Medical relations
5
From Japan
On 2017-04-05 09:07:38
I like it very much. There is opinion of both sides in other postings and it reflects morphological individual difference. I think that there is no use for not knowing without using it. For me the position of the convex lens was perfect.
1 2 3
Customer Who Viewed This Item Also Viewed
Reading Glasses UN26
Safety Glasses
Safety Glasses
Senior Glasses
Glasses Binocular
Library compact 4230
Library  4470
ESCHENBACH Working Loupe
Head Loupe (Glasses)
Make-up glasses
Library compact light 4140