Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nylon Cutter Basic

Nylon Cutter Basic
Sales Price: 12.99 SGD
Review Rating: 3.89
9 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Slightly hard grass cutting
2
From Japan
On 2017-11-27 16:23:15
Compared with the nylon cord cutter manual feed / entrainment type cutter round, it can be wound long Why will it be exhausted as a result Why use stopped It may be nice to take a leisurely weed at low speed rotation.
Code is very difficult to inefficient
2
From Japan
On 2017-06-07 17:10:36
Because the shape is bad, it is very difficult to put out a cord. It is cheap and light, but it is an impression that it is for people who truly have little area to cut. Also, the shape of the exit part of the cord is rounded so that the cord is not easily broken, but there are cases where welding is done without cutting from the root regardless.
This review is about item#60958371.
Harvest
5
From Japan
On 2017-01-16 12:07:39
Although code exchange was troublesome, I tried several kinds, but after all, the automatic delivery type was troublesome and it took time and trouble to fix, and at last the product was simple. It can be used easily and reliably.
This review is about item#60958371.
Mowing
4
From Japan
On 2016-09-07 14:05:17
Almost every weekend we are working on farmland mowing. The advantage of this product is cheap, lightweight, simple. If you dare to mention a disadvantage, mixing of mud grass is easy to accumulate on the outer periphery of the inside of the bowl, so eccentric blurring is likely to occur (so that fingers with handles will hurt). If you put out the four cords against the notice, it has no shakiness and the sharpness of the cord has become long.
This review is about item#60958371.
Electric wiring
4
From Japan
On 2016-07-29 18:07:48
There is no problem in initial use. Durability in long-term use is unknown.
This review is about item#60958371.
Hunting, cutting grass growing on the gravel road
3
From Japan
On 2016-07-13 18:19:21
It is light and the price is affordable. Since the main is a bamboo blade, we are using it on a sub-cutter.
This review is about item#60958371.
Mowing of small weeds
5
From Japan
On 2016-05-25 19:04:37
I have been using this product forever. Even if it is simple and easy to use it is useful.
This review is about item#60958371.
Mowing in the walls and stone-rich places
5
From Japan
On 2016-04-15 16:08:59
Simple and easy to use. If the code becomes short or broken, you have to shift the hole through which the cord passes by hand, but it is easy and there is no breakdown than anything else. Soft grass is easy to prune. Because there are two mowers, they are used properly in the place of the chip saw and the place of use.
This review is about item#60958371.
Used for cutting grasses such as fields and riverbeds
5
From Japan
On 2013-08-02 17:53:32
Frequently, when the code decreases with other products, it is automatically unwound as much as it is reduced, and there are things where the code is fed out by hitting it on the ground, but it is difficult to replenish the code or biting in It is difficult to assemble it after disassembling. It's both good and bad. Until now, I have used manual and automatic, but simple is still the best. I have to stop and stop the machine once, but it is reliable, there is no breakdown. For the reason I have been using this product for a while.
This review is about item#60958371.
1
Customer Who Viewed This Item Also Viewed
Nylon Cutter Insertion
Nylon Cutter
Winding Nylon Cutter
Mowing Nylon Cutter Round
Nylon cutter plugin
Full Auto Nylon Cutter 3
Nylon cutter plugin
Plug-in nylon cutter
Manual rotor
Elba A
  • Elba A
  • Sanyo Metal Works (ERBA)
  • 18.99 SGD
  • 4.000000(1)
Elba B