Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Sensor Map (SH)

Sensor Map (SH)
Sales Price: 49.99 SGD
Review Rating: 4.82
11 Customer Reviews
5 star 9
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
CX-8 spare parts
5
From Japan
On 2018-04-13 15:16:25
Scheduled cleaning every 5000 km. As a reserve for replacement if necessary.
This review is about item#64024405.
Maintenance of CX-5 XD KE 2 series
5
From Japan
On 2018-01-23 00:28:35
Although it was cleaning every 10,000 km, it has reached 70,000 km and it is replaced with a new one. Manufacturers do not designate periodic exchanges, but they are carried out with self-satisfaction and self-responsibility. I like the best engine, I want to continue riding for a long time.
This review is about item#64024405.
Car maintenance
4
From Japan
On 2017-07-10 21:02:25
I bought it with what I had on the vehicle and planning to use it in rotation. I replaced it with 50,000 kilometers, but I feel that the knock when departing with a half clutch has decreased. There was no noticeable change in idling and acceleration.
This review is about item#64024405.
Intensifier pressure sensor of the Atenza Wagon (GJ)
5
From Japan
On 2017-05-30 00:47:29
Since there was an introduction at Minkara, I tried to exchange it at 51,000 km. As a result, the engine became smooth (feeling that the colorless sound was reduced). It may be reasonable because it was a terrible carbon adhesion when looking at the removed sensor. The value of exchanging is great.
This review is about item#64024405.
Change sensor
5
From Japan
On 2017-05-22 16:25:45
It was exchanged at 7 thousand kilometers before, this time it is 14 thousand kilometers and it is an exchange. I can feel the change in engine response.
This review is about item#64024405.
For regular replacement
5
From Japan
On 2017-04-03 15:08:42
I regularly remove this part and clean it, but I purchased a spare in case of emergency. It happened to happen, but it was very helpful to have it shipped the day.
This review is about item#64024405.
Maintenance of the sensor
4
From Japan
On 2017-02-27 17:18:55
Replace sensor soon soiled. Is the same as the current one and the model number? Because the design of the character array was changed, I was surprised mistakenly that I made a mistake.
This review is about item#64024405.
Early exchange in own usage situation.
5
From Japan
On 2016-06-15 14:15:17
As it was covered with soot as a result of repeated confirmation at 4,000 kilometers, slight ride, warm-up, idling, stop & go repeated, I was scared of sensor breakage and so I exchanged at 8,000 kilos, even if the rattle sound is quite small even when cold became.
This review is about item#64024405.
Engine maintenance
5
From Japan
On 2015-10-05 14:59:47
It is contamination of this sensor that was getting into the topic as one cause of engine malfunction on the Internet. Reaction with no problem as to dealer etc confirmed the truth several times. The mileage has reached 53000 km. Unexpectedly removed from the engine and I saw the degree of soiling It is almost packed. I tried cleaning with a toothpick or a cotton swab but now it is one. So it was relatively inexpensive and replaced with a new one. Variations in idling and carcass sounds during acceleration decreased.
This review is about item#64024405.
Regular maintenance
5
From Japan
On 2014-10-13 14:33:17
Ideal for spare after traveling thousands of kilometers. Soot adheres such as sludge and regular maintenance is satisfied with this.
This review is about item#64024405.
Maintenance of cars
5
From Japan
On 2014-09-06 13:28:37
Purchased for maintenance of own car. After replacement, the diesel engine became lighter.
This review is about item#64024405.
1
Customer Who Viewed This Item Also Viewed
Valve air (99)
Panel (L), Suitsuchi
Trunk, trunk room sub
Panel (R), Suitsuchi
Suitsuchi, power window
FRONT SKIRT (QG)