Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bearing entering iron car only

Bearing entering iron car only
Sales Price: 4.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Industrial sewing machine presser lifting
5
From Japan
On 2018-10-21 23:33:17
It was used as a guide to slightly change the pulling direction of 2 mm stainless steel wire. I am in good health.
This review is about item#75821882.
Replacing only the car part of the door roller of the old door pulled door of the super old
5
From Japan
On 2018-07-18 18:02:10
The super old old doorway entrance door of Yamanashi prefecture's parents house stopped moving smoothly. The roller car bearings came up. I mailed that I wanted to get a replacement item for the door roller to the door maker, but it was without sound. I asked the company of the door roller special-purpose manufacturing contractor to attach a drawing and found that the car was small and could not be manufactured. At such a time, I found only a car of the same diameter at the site of Monotaro. Also, as I looked for an axle with the same diameter as the shaft hole 5 mmφ of the car, I was selling it with processing that cuts to the specified length, so I bought it with a cut with a length of 16 mm. With this, we were able to accomplish the replacement of only the car part of the door roller assembly 4 by oneself. Since the shaft was a little loose, it was fixed to the car with epoxy adhesive. In addition, the height adjustment screw of the car: 30 mm long x 5 mm φ has a groove near the head. Because this is old and it seems unreliable, we made four new disk grinders and iron file. I am very satisfied with the result. But since I have not returned to my parents house yet, I have not attached it to the door itself.
This review is about item#75821891.
I used it as a wire receiver
5
From Japan
On 2016-08-25 18:15:38
I suppose it was originally a door roller, but this time I used wires to tension the wire. I am satisfied with my successful use.
This review is about item#75821916.
For metal wire rope guide
3
From Japan
On 2016-04-06 22:56:43
Since I have not used it yet, I can not evaluate it. But since the price was right, we would like to use various things.
This review is about item#75821891.
1
Customer Who Viewed This Item Also Viewed
Pulley 90
Steel Pulley Snatch
Sash Roller Wheel
Resin Bearing EU
Brass car only
Bearing input sheave
Pulley Wheel
Normal sheave
Usually sieve stainless
Cast car only
6 'Nylon car only
Round belt roller
Nylon Door Rollers
LP Plus car only
Unladed weight car C-1100 series V type