Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Dial Gauge

Dial Gauge
Sales Price: 41.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
experimental
5
From Japan
On 2018-09-10 15:17:20
I bought it to measure the deformation of the body, but it is convenient because the stroke is long and it does not need to be changed.
This review is about item#68541566.
Measure wheel rotation of off-road motorcycle
5
From Japan
On 2017-07-14 19:26:40
Assuming the rim deflection measurement of the spoke wheel, purchased along with the company's fine-adjustment base. As an amateur for the first time to use, when placing the stand simply and hitting the dial gauge to the object to be measured, I notice after the purchase that the platform will tilt with repulsion more than I thought. We also have 1.6 kg weight I am a little surprised because it is gussily. When using it, it is necessary to fix with a magnetic force with a deflection base that holds the wheel. Even if you use the gauge itself for the first time, it is enough for Sunday mechanic to see easily.
This review is about item#68541566.
Core in the lathe, propeller shaft measurement
4
From Japan
On 2017-05-08 19:55:02
I use it with a magnetic stand. Making is also good. It is truly Mr. Shinwa.
This review is about item#68541566.
1
Customer Who Viewed This Item Also Viewed
Standard Dial Indicator, 0.01mm Scale Mark
Magnet Stand
Dial Indicator
0.001mm Dial Indicator
Small Dial Gauge
Dial Indicator, Small
Dial Test Indicator
Long-Stroke Dial Indicator
Dial Indicator, Small
Parts for Dial Gauge Standard type
Dial Gauge
Dial Indicator