Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of End Caps, Square-Pipe

End Caps, Square-Pipe
Sales Price: 1.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used to make a table!
5
From Japan
On 2018-02-07 05:23:39
I worried whether it fits the inner diameter of the square pipe, but it fits well!
This review is about item#75860373.
Adjusting the height of the work table
5
From Japan
On 2018-01-19 14:48:39
The fit to the pipe was also not loose and not too loose. I just wanted to raise the height as much as 1 cm, so it was just fine.
This review is about item#75860346.
Leg extension of ready-made products
5
From Japan
On 2018-01-16 20:03:26
Since the material is plastic, I had anxiety before putting on it, but once it was assembled it was firmly fixed and worrying anxiety. It was over the full mark with the dimensions as shown.
This review is about item#75860346.
Parts replacement for long-legged legs
4
From Japan
On 2017-12-02 12:02:41
Because the long part being used for years has broken the plastic part of the legs due to aged deterioration, the screw of the adjuster stopped stopping, so I bought it for that replacement. It is convenient because this item has an adjuster attached from the beginning. Just because the material of the adjuster is also a solid plastic, I think it was better if the part in contact with the floor was made of rubber.
This review is about item#75860364.
Furniture leg end cap
4
From Japan
On 2017-06-17 14:33:31
Just size square pipes of 25 x 25. There is an adjuster, it can correspond to floor unevenness. A commercially available cushioning material is affixed when the seat plate is a little bigger.
This review is about item#75860364.
1
Customer Who Viewed This Item Also Viewed
End Cap
The end cap (H8)
Square pipe insert
Corner in the cap
SQ-223 to 228
BC 860
  • BC 860
  • Miyoshi Kikai (former Miyoshi Pijon)
  • 21.99 SGD
Square End Caps