Buy more than* S$200* and get FREE SHIPPING
---
*Notice*
Due to the maintenance, we will close our website from July 21,2018 10PM to July 22, 2018 4AM JST.
All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Wood Cutting Saw Blade

Wood Cutting Saw Blade
Sales Price: 41.99 SGD
Review Rating: 3.88
8 Customer Reviews
5 star 2
4 star 4
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Roughing of wood, removal of sapwood parts of natural wood
4
From Japan
On 2018-03-14 11:29:08
Buy the second one. Wear is extremely fast for hard wood and lid parts. Reprinting can be done several times. It is unsuitable because it wears out considerably when planar finishing is tried. Compared with scraping with an engine chain saw, it is advantageous that there is no adhesion of oil. Although the hole diameter spacer is attached, the use of the side handle stabilizes with the 125 mm disc grinder. Since shavings scatter over a radius of 5 m or more, a simple apron and face guard are installed and working. People who are not used to handling grinders will have kickbacks. Because it can not endure full-scale work and continuous use, it is suitable for the price.
This review is about item#75805441.
Inner surface drilling of natural wooden vessels
4
From Japan
On 2017-12-19 21:46:01
Since the cutting edge did not seem to be cut from the time of purchase, specification after polishing with Φ 4 mm file for chainsaw. Sakura wood, Sawara material, sharpness was good. Frequent polishing is required as well as chain blades.
This review is about item#75805441.
Mori mover of woodwork
2
From Japan
On 2017-07-13 14:05:18
I can not use it because it is coarse and precise does not come out! I want you to display for rough cutting and sell it!
This review is about item#75805441.
For processing natural wood
3
From Japan
On 2017-06-19 20:55:40
From the first use, it was slightly cloudy to the blade, it got attached, and the sharpness seemed to be suitable for the price.
This review is about item#75805441.
Sculpture rough carving
4
From Japan
On 2017-01-31 13:00:32
Although it was a hammer drill on the bottom of a hollow carving, it was a feeling to drop an extra part due to a bit of a flea shape but the exterior cutter can be scraped in one more step and the cutting surface is also beautiful so immediately the real carving It is useful for you
This review is about item#75805441.
For engraving the seat plate of the chair
4
From Japan
On 2016-10-11 01:24:31
The appearance is just sharpening by bending a metal sheet, but it was sufficient sharpness to gouge the wood. It is unknown how long the sharpness will last, but for now we were able to use it without problems.
This review is about item#75805441.
Sharpening of curved surface of wooden dishes
5
From Japan
On 2016-08-14 22:12:00
When I saw this product, the first thing I thought was that I used Japanese as "necessary enough" for such occasions. As I looked at it, it is not a special tip attached, it is a simple item with punching and processing a steel plate with a blade. But if you use it as a hand-held tool when attached to an ordinary grinder you have with hands, it's also good sharpness and this is enough. I am satisfied.
This review is about item#75805441.
Kindergarten machine
5
From Japan
On 2014-05-21 18:01:03
Since it is an assembling work only with logs, it was saved for subtle work in the meshing part.
This review is about item#75805441.
1
Customer Who Viewed This Item Also Viewed
Cutter Chainsaw Blade
Meritter, For Universal Groove Cuts
Disc Grinder Protector
Diamond grooving cutter
Counterbore cutter
Birds type chisel round
Carbide Aegli cutter
570g hammer with a claw
Children gloves pure cotton