Buy more than* S$200* and get FREE SHIPPING
Note
Due to the maintenance, we will close our website on 2020/1/26 PM 08:00-09:00 JST.
All customers cannot shop on our website during the time. Thank you.

Customer Reviews of T-HandleTap Wrench

T-HandleTap Wrench
Sales Price: 14.99 SGD
Review Rating: 3.67
9 Customer Reviews
5 star 3
4 star 2
3 star 2
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Maintenance of the bike
5
From Japan
On 2019-02-04 18:20:13
I purchased this so that I could tap with ASSY without completely disassembling. The usable width of the tap is wider than that of other manufacturers, yet the size is almost the same, so it is easy to use. There was a scene to use immediately after arriving, but it is very easy to use. Price is cheap and is recommended.
This review is about item#86927294.
Tap in a small place
3
From Japan
On 2018-06-06 15:17:18
The wide range of sizes that can be chucked is a beauty point. Since the chuck is internally held by a small spring, if it is scattered, there is a danger of losing parts. Since the handle is only thrusting the round bar, the feeling of use is not good. There is a countersunk screw to fix the handle, but it is better not to be in a narrow place. Even if you screw tightening the countersunk screw with an eye-catching mark, you will experience a misalignment when you turn 180 °. After all, you should cut grooves in the center to make a ball lock, and stop at both ends. A washer for M6 was welded to this countersunk screw as a first aid so that it could be tightened and loosened by hand. If you can be tightened with parts of design like micrometer ratchet stops, your satisfaction may be a bit better.
This review is about item#86927294.
Fix wheel nut
3
From Japan
On 2018-02-13 13:39:29
I bought it for the M12 tap, but it is troublesome to have the handle fixed with screws. Also, it was surprising that many chips were mixed during cutting! Regrettable though performance was not a problem.
This review is about item#86927285.
Thread cutting
2
From Japan
On 2017-02-05 18:07:30
Certainly M5 can get through. Whether the handle is too short at M8 or higher.
This review is about item#86927276.
Sheet metal work
2
From Japan
On 2016-05-09 21:46:20
Although it became correspondence from m4, the tap purchased at the same time can not be firmly fixed and it is in a state of loose state. I could use it properly in m6, but I was sorry though I made it.
This review is about item#86927276.
I used it when I used taps.
4
From Japan
On 2016-05-07 22:11:12
I bought it at the same time, I used it to use M10's tap. Firmly fixed, handles can also move so it was useful when you wanted to apply force strongly.
This review is about item#86927285.
Tapping
4
From Japan
On 2016-04-07 22:34:49
It is a bit small to put strength.
This review is about item#86927285.
Tap stand of aluminum building material
5
From Japan
On 2016-03-13 15:04:48
As for the TRS-4, as shown in the posted photograph, the chuck shape is different only for this type. Since the insertion slot is square, the tap does not slip and is retained. It can also be recommended because the material is also good quality cut-out material. Originally I bought TRS-1 for the purpose of 4φ, but changed and confirmed.
This review is about item#86927294.
Product name as w
5
From Japan
On 2015-10-07 15:08:04
I think that it belongs to reasonable prices, but I am satisfied with a solid build more than I expected.
This review is about item#86927267.
1
Customer Who Viewed This Item Also Viewed
Tap handle
SF tap wrench (ratchet type)
Ratchet Tap Holder
T Type Tap Holder
T Type Tap Holder
T type holder
Swing plug
Tap Holder
Tap handle
T-HandleTap Wrench