Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of D series tension coil spring

D series tension coil spring
Sales Price: 27.99 SGD
Review Rating: 5.00
1 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Microwave door spring restoration
5
From Japan
On 2018-05-03 17:24:26
The spring which pulled the door of the microwave oven has been cut as "Batcheoon!", As I opened it, the head of the tension spring was tearing off one side. I am tired. I measured the spring that was left and I bought it looking for something similar. In fact it should be chosen by tensile strength etc, but since there was no way to measure it, we purchased it judging from coil diameter and wire diameter, free length. As I arrived, the diameter of the coil wire diameter was perfect, but it seems that the number of turns was less than a turn, it became slightly shorter, but as it is a spring, it was installed as it was, is. Although it seems to be somewhat tighter than originally, I do not understand it with the feeling of using it. Since there are 4 bottles, there are also 3 spares, and even if it seems that fatigue will come out early, perhaps it will not be exhausted perhaps, but when that time comes, I think I should buy the spring of the original length.
This review is about item#1367433.
1
Customer Who Viewed This Item Also Viewed
Tension Spring Hp, Piano Wire
Tension Coil Spring
Tension Coil Spring FP Piano Wire
Extension Coil Spring
Tension Coil Spring
Tension Coil Spring
Tension Coil Spring
Length coil spring
Extension Spring
Hanging spring