Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Head Loupe (Glasses)

Head Loupe (Glasses)
Sales Price: 29.99 SGD
Review Rating: 3.80
10 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Fine work
4
From Japan
On 2018-11-10 16:38:04
There is also a microscope, but I will use this if it is not fine work.
This review is about item#5853898.
Making a gimmick for fishing
2
From Japan
On 2017-09-29 11:06:21
When you set it normally, you will be away from the eyes, so you will have to go up. This makes the eyes tired. The lens up mechanism may be present, but when down it seems better usability if it goes down a little more. Therefore, I stop directly on the nose pad with a rubber band, I do not feel the necessity of up. If attached lenses can also be selected as 1.5, 1.7, 2.0 ◎.
This review is about item#5853898.
Fine polish
5
From Japan
On 2017-09-11 16:27:47
For fixation around forehead, than usual glasses type Neighborhood does not hurt, wearing clothes are good and easy to see.
This review is about item#5853898.
Soldering
4
From Japan
On 2017-07-30 15:51:21
The 2.5-fold lens that was supposed for the soldering work is narrow viewing or it is crazy because distortion around it is concerned, so I am regularly using 2.0 times. It is better that there is no pressure feeling lighter than the headband type I used to use.
This review is about item#5853898.
Maintenance of automobiles
5
From Japan
On 2017-06-20 07:23:42
I used glasses in the distance (middle-near) during maintenance, but I was good at borrowing a hazuki because the focus did not fit well in a reasonable place, but I tried buying it as a wash in trouble due to work. Although fixing is sweet in other reviews, although the mounting position of the lens is incorrect, I thought that it was useless with a wrong shaky but I fixed it. It was.
This review is about item#05853898.
Repair of electrical board etc.
5
From Japan
On 2017-02-27 12:51:08
It is light and comfortable to wear, looks great and looks very handy.
This review is about item#5853898.
Precision work
2
From Japan
On 2017-01-19 10:00:30
It is good to be able to exchange the magnification. If the fixation is too loose to face downwards, the lens will tilt and it is very hard to use.
This review is about item#5853898.
Precision work
1
From Japan
On 2016-10-01 11:59:15
The focal length is too close (about 10 cm in front of you). Since the place to fix the lens is loose, the lens will also tilt as it becomes bent forward w
This review is about item#5853898.
For detailed work
5
From Japan
On 2015-10-14 15:35:23
When the company has detailed work, the father of the president also uses it personally to read the newspaper. It is popular because it is light and easy to work with.
This review is about item#05853898.
Miniature painting
5
From Japan
On 2015-05-08 12:47:57
Very light, the structure is very simple and very good. At first, I bought a head loupe with LED light, but it was somewhat heavy, and the adjustment part of the band was broken so it was a purchased item.
This review is about item#05853898.
1
Customer Who Viewed This Item Also Viewed
Head Magnifying Glass
Glasses Loupe LED
Glasses For Loupe, Binocular
Binocular Loupe
Glasses Binocular
Glasses Magnifier
Binocular Loupe Clip
ESCHENBACH Working Loupe
Head Magnifying Glass
Binoculars Glasses Loupe (Frame Time)
PEGAVIEW
HEAD LOUPE SHI-RA-RA R1178-03