Buy more than* S$200* and get FREE SHIPPING

* Announcement of Payment Method Change *
Credit card payment is now available via Paypal platform.
Paypal account is not essential.
In addition to Visa and MasterCard, American Express, and Discover are also available now.
(Availability of each brand in your country follows PayPal policy)

Customer Reviews of Tool Wagon

Tool Wagon
Sales Price: -
Review Rating: 4.00
10 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For interior work
4
From Japan
On 2018-04-12 19:05:43
Because it is interior construction work as you work in a small space Do not try to find tools or tools at all I bought this because there are so many. Putting it in the closet already There is no refreshment, you can concentrate on work. However, Whether the length was slightly different or the casters did not reach the floor one place So I adjusted with bolt. It was good that it was able to be done.
This review is about item#29978375.
Daily work of car
5
From Japan
On 2018-03-25 19:10:11
Although it is inexpensive, it can be used with confidence since the body and the roller part are also firmly made. Even if it says anything, it is lightweight and it is smooth because it moves smoothly.
This review is about item#29978375.
Organizing tools
3
From Japan
On 2017-12-19 22:07:25
I got it because I was able to handle with genuine parts. no problem.
This review is about item#29978375.
During wood work
2
From Japan
On 2017-11-24 09:02:20
I tried to assemble it as soon as it arrived but because the pipe did not enter abnormally tightly it warmed up with a dryer and assembled it. There was also a review that was wobbly but it was solid enough to worry that it did not fit deeply.
This review is about item#29978375.
On-site workbench
5
From Japan
On 2017-10-20 16:16:26
Although it is used at the site of steel material processing, storage is finely divided and it is easy to use. It is popular that we can move with casters. Movement is also light.
This review is about item#29978375.
When polishing work, body coating
5
From Japan
On 2017-10-19 14:57:31
The set of tools fits and the movement is easy. I am satisfied because strength is enough.
This review is about item#29978375.
During repair and maintenance of machine
5
From Japan
On 2017-10-07 16:58:04
I think the making of the product itself is reasonable. If you can add another step with optional parts etc., private use will improve usability, so please consider.
This review is about item#29978375.
Car maintenance
5
From Japan
On 2017-07-13 09:58:41
Light response The response at maintenance is improved and it is highly efficient Difficult point is that the can holder is shallow
This review is about item#29978375.
To facilitate on-site work
2
From Japan
On 2017-07-09 12:31:53
I tried to assemble it, but there seems to be a slight wobble and seems to be bad stability. It is true that there is uneasiness as to whether it will stabilize if a heavy tool is placed, or is unstable so that it will collapse. Since I move on a date, I do not think it is cheap how that wobble is also cheap, so I would like to use that around and tell the impression again.
This review is about item#29978375.
During sheet cleaning
4
From Japan
On 2017-02-07 08:48:21
It is used to put spray etc during flameproof sheet cleaning work. From usability, price, I think that it is a reasonable product. However, there is a risk that the spray will collapse because the depth of the cup containing the spray is shallow.
This review is about item#29978375.
1